This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运行CSL库文件中的mcbsp的例程显示TEST FAILED



(在CCS5.5 的编译环境下,用的是C5509开发板)

我在编译 运行 C55xxCSL\examples\generic5509\csl\mcbsp\mcbsp1 里面的McBSP的工程之后,下面提示 TEST FAILED。

并且,当我把鼠标放在taskFxn()这个函数上时,显示

请问为什么会这样?

  • (附件中顺便附上了整个工程代码)

    主程序源码如下:

    /*
    * Copyright (C) 2003 Texas Instruments Incorporated
    * All Rights Reserved
    */
    /*
    *---------main_mcbsp1.c---------
    * In this example, the MCBSP is configured in digital loopback
    * mode, with 32 bit data transfer, in multi-frame mode, using
    * sample rate generator to sync frames
    */
    #include <stdio.h>

    #include <csl.h>
    #include <csl_mcbsp.h>
    #include <csl_irq.h>


    //---------Global constants---------
    #define N 10

    //---------Global data definition---------

    MCBSP_Config ConfigLoopBack32= {
    MCBSP_SPCR1_RMK(
    MCBSP_SPCR1_DLB_ON, /* DLB = 1 */
    MCBSP_SPCR1_RJUST_RZF, /* RJUST = 0 */
    MCBSP_SPCR1_CLKSTP_DISABLE, /* CLKSTP = 0 */
    MCBSP_SPCR1_DXENA_NA, /* DXENA = 0 */
    MCBSP_SPCR1_ABIS_DISABLE, /* ABIS = 0 */
    MCBSP_SPCR1_RINTM_RRDY, /* RINTM = 0 */
    0, /* RSYNCER = 0 */
    MCBSP_SPCR1_RRST_DISABLE /* RRST = 0 */
    ),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO, /* FREE = 0 */
    MCBSP_SPCR2_SOFT_NO, /* SOFT = 0 */
    MCBSP_SPCR2_FRST_RESET, /* FRST = 0 */
    MCBSP_SPCR2_GRST_RESET, /* GRST = 0 */
    MCBSP_SPCR2_XINTM_XRDY, /* XINTM = 0 */
    0, /* XSYNCER = N/A */
    MCBSP_SPCR2_XRST_DISABLE /* XRST = 0 */
    ),
    MCBSP_RCR1_RMK(
    MCBSP_RCR1_RFRLEN1_OF(0), /* RFRLEN1 = 0 */
    MCBSP_RCR1_RWDLEN1_32BIT /* RWDLEN1 = 5 */
    ),
    MCBSP_RCR2_RMK(
    MCBSP_RCR2_RPHASE_SINGLE, /* RPHASE = 0 */
    MCBSP_RCR2_RFRLEN2_OF(0), /* RFRLEN2 = 0 */
    MCBSP_RCR2_RWDLEN2_8BIT, /* RWDLEN2 = 0 */
    MCBSP_RCR2_RCOMPAND_MSB, /* RCOMPAND = 0 */
    MCBSP_RCR2_RFIG_YES, /* RFIG = 0 */
    MCBSP_RCR2_RDATDLY_2BIT /* RDATDLY = 0 */
    ),
    MCBSP_XCR1_RMK(
    MCBSP_XCR1_XFRLEN1_OF(0), /* XFRLEN1 = 0 */
    MCBSP_XCR1_XWDLEN1_32BIT /* XWDLEN1 = 5 */

    ),
    MCBSP_XCR2_RMK(
    MCBSP_XCR2_XPHASE_SINGLE, /* XPHASE = 0 */
    MCBSP_XCR2_XFRLEN2_OF(0), /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT, /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB, /* XCOMPAND = 0 */
    MCBSP_XCR2_XFIG_YES, /* XFIG = 0 */
    MCBSP_XCR2_XDATDLY_2BIT /* XDATDLY = 0 */
    ),
    MCBSP_SRGR1_RMK(
    MCBSP_SRGR1_FWID_OF(1), /* FWID = 1 */
    MCBSP_SRGR1_CLKGDV_OF(1) /* CLKGDV = 1 */
    ),
    MCBSP_SRGR2_RMK(
    MCBSP_SRGR2_GSYNC_FREE, /* FREE = 0 */
    MCBSP_SRGR2_CLKSP_RISING, /* CLKSP = 0 */
    MCBSP_SRGR2_CLKSM_INTERNAL, /* CLKSM = 1 */
    MCBSP_SRGR2_FSGM_DXR2XSR, /* FSGM = 0 */
    MCBSP_SRGR2_FPER_OF(15) /* FPER = 0 */
    ),
    MCBSP_MCR1_DEFAULT,
    MCBSP_MCR2_DEFAULT,
    MCBSP_PCR_RMK(
    MCBSP_PCR_IDLEEN_RESET, /* IDLEEN = 0 */
    MCBSP_PCR_XIOEN_SP, /* XIOEN = 0 */
    MCBSP_PCR_RIOEN_SP, /* RIOEN = 0 */
    MCBSP_PCR_FSXM_INTERNAL, /* FSXM = 1 */
    MCBSP_PCR_FSRM_EXTERNAL, /* FSRM = 0 */
    MCBSP_PCR_CLKXM_OUTPUT, /* CLKXM = 1 */
    MCBSP_PCR_CLKRM_INPUT, /* CLKRM = 0 */
    MCBSP_PCR_SCLKME_NO, /* SCLKME = 0 */
    0, /* DXSTAT = N/A */
    MCBSP_PCR_FSXP_ACTIVEHIGH, /* FSXP = 0 */
    MCBSP_PCR_FSRP_ACTIVEHIGH, /* FSRP = 0 */
    MCBSP_PCR_CLKXP_RISING, /* CLKXP = 0 */
    MCBSP_PCR_CLKRP_FALLING /* CLKRP = 0 */
    ),
    MCBSP_RCERA_DEFAULT,
    MCBSP_RCERB_DEFAULT,
    MCBSP_RCERC_DEFAULT,
    MCBSP_RCERD_DEFAULT,
    MCBSP_RCERE_DEFAULT,
    MCBSP_RCERF_DEFAULT,
    MCBSP_RCERG_DEFAULT,
    MCBSP_RCERH_DEFAULT,
    MCBSP_XCERA_DEFAULT,
    MCBSP_XCERB_DEFAULT,
    MCBSP_XCERC_DEFAULT,
    MCBSP_XCERD_DEFAULT,
    MCBSP_XCERE_DEFAULT,
    MCBSP_XCERF_DEFAULT,
    MCBSP_XCERG_DEFAULT,
    MCBSP_XCERH_DEFAULT
    };

    /* Define a MCBSP_Handle object to be used with MCBSP_open function */
    MCBSP_Handle mhMcbsp;
    Uint32 xmt[N], rcv[N];
    volatile Uint16 XfrCnt = 0;
    Uint16 err = 0;
    Uint16 old_intm;
    Uint16 rcvEventId, xmtEventId;

    //---------Function prototypes---------

    /* Reference start of interrupt vector table */
    /* This symbol is defined in file, vectors.s55 */
    extern void VECSTART(void);

    // Interrupt Service Routine Prototypes
    interrupt void writeIsr(void);
    interrupt void readIsr(void);

    void taskFxn(void);

    //---------main routine---------
    void main(void)
    {
    Uint16 i;

    /* Initialize CSL library - This is REQUIRED !!! */
    CSL_init();

    /* Set IVPD/IVPH to start of interrupt vector location */
    printf("%d\n", &VECSTART);
    IRQ_setVecs((Uint32)(&VECSTART));

    for (i = 0; i <= N - 1; i++) {
    xmt[i] = ((Uint32)i << 17) + i;
    rcv[i] = 0;
    }

    /* Call function to effect transfer */
    taskFxn();
    }

    void taskFxn(void)
    {
    Uint16 i;

    old_intm = IRQ_globalDisable();

    /* Open MCBSP Port 0 and set registers to their power on defaults */
    mhMcbsp = MCBSP_open(MCBSP_PORT0, MCBSP_OPEN_RESET);

    /* Get EventId's associated with MCBSP Port 0 receive and transmit */
    /* The event Id's are used to communicate with the CSL interrupt */
    /* module functions. */
    rcvEventId = MCBSP_getRcvEventId(mhMcbsp);
    xmtEventId = MCBSP_getXmtEventId(mhMcbsp);

    /* Clear any pending receive or transmit interrupts */
    IRQ_clear(rcvEventId);
    IRQ_clear(xmtEventId);

    /* Place address of interrupt service routines at */
    /* associated vector location */
    IRQ_plug(rcvEventId, *readIsr);
    IRQ_plug(xmtEventId, *writeIsr);

    /* Write values from configuration structure to MCBSP control regs */
    MCBSP_config(mhMcbsp, &ConfigLoopBack32);

    /* Enable the MCBSP receive and transmit interrupts */
    IRQ_enable(rcvEventId);
    IRQ_enable(xmtEventId);

    /* Start Sample Rate Generator and Frame Sync */
    MCBSP_start(mhMcbsp,
    MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
    0x300
    );

    /* Enable MCBSP transmit and receive */
    MCBSP_start(mhMcbsp,
    MCBSP_RCV_START | MCBSP_XMIT_START,
    0
    );

    /* Prime MCBSP transmit */
    while(!MCBSP_xrdy(mhMcbsp)){
    ;
    }
    MCBSP_write32(mhMcbsp,xmt[XfrCnt]);

    /* Enable all masked interrupts */
    IRQ_globalEnable();

    /* Wait for transfer of data */
    while (XfrCnt < 10) {
    ;
    }

    /*------------------------------------------*\
    * Compare values
    \*------------------------------------------*/
    for(i = 0; i <= N - 1; i++){
    if (rcv[i] != xmt[i]){
    ++err;
    break;
    }
    }

    printf ("%s\n",err?"TEST FAILED" : "TEST PASSED");

    /* Restore old value of INTM */
    IRQ_globalRestore(old_intm);

    /* We're done with MCBSP, so close it */
    MCBSP_close(mhMcbsp);
    }

    interrupt void writeIsr(void)
    {
    /*
    * Disable this ISR's interrupt before the write to the McBSP
    * since another interrupt will be generated as soon as the write
    * completes, which happens very quickly due to the loopback to
    * the McBSP receive.
    */
    IRQ_disable(xmtEventId);
    MCBSP_write32(mhMcbsp,xmt[XfrCnt]);
    }

    interrupt void readIsr(void)
    {
    rcv[XfrCnt] = MCBSP_read32(mhMcbsp);
    ++XfrCnt;

    if (XfrCnt == N) {
    IRQ_disable(rcvEventId);
    IRQ_disable(xmtEventId);
    MCBSP_reset(mhMcbsp);
    }
    else {
    IRQ_enable(xmtEventId);
    }
    }

    经过调试发现,在第二次数据传送过程中,发数据中断服务函数(黄色)并没有执行,而是直接执行了收数据中断服务函数(绿色),所以收端的第二个数据有误(如下图所示)

    哪位大神知道这是为什么吗?

    mcbsp1.zip
  • 这个问题我自己解决了。

    下面这个函数中:

    void taskFxn(void)
    {
        Uint16 i;
    
        old_intm = IRQ_globalDisable();
      
        /* Open MCBSP Port 0 and set registers to their power on defaults */
        mhMcbsp = MCBSP_open(MCBSP_PORT2, MCBSP_OPEN_RESET);
    
        /* Get EventId's associated with MCBSP Port 0 receive and transmit */
        /* The event Id's are used to communicate with the CSL interrupt   */
        /* module functions.                                               */
        rcvEventId = MCBSP_getRcvEventId(mhMcbsp);
        xmtEventId = MCBSP_getXmtEventId(mhMcbsp);
       
        /* Clear any pending receive or transmit interrupts */
        IRQ_clear(rcvEventId);           
        IRQ_clear(xmtEventId);
           
        /* Place address of interrupt service routines at */
        /* associated vector location  */
        IRQ_plug(rcvEventId, &readIsr);            
        IRQ_plug(xmtEventId, &writeIsr);
       
        /* Write values from configuration structure to MCBSP control regs */
        MCBSP_config(mhMcbsp, &ConfigLoopBack32); 
    
        /* Enable the MCBSP receive and transmit interrupts */
        IRQ_enable(rcvEventId);          
        IRQ_enable(xmtEventId);
    
       /* Start Sample Rate Generator and Frame Sync */
       MCBSP_start(mhMcbsp, 
                   MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC, 
                   0x300
                   );
    
        /* Enable MCBSP transmit and receive */
        MCBSP_start(mhMcbsp, 
                    MCBSP_RCV_START | MCBSP_XMIT_START, 
                    0
                   );
       
       /* Prime MCBSP transmit */
        while(!MCBSP_xrdy(mhMcbsp)){
          ;
        }
     MCBSP_write32(mhMcbsp,xmt[XfrCnt]);
        
    	/* Enable all masked interrupts */
       	IRQ_globalEnable();
     
        /* Wait for transfer of data */
        while (XfrCnt < 10) {
            ;
        }
       
        /*------------------------------------------*\
         * Compare values 
        \*------------------------------------------*/   
        for(i = 0; i <= N - 1; i++){
            if (rcv[i] != xmt[i]){
                ++err;
                break;
           }
        }
    
        printf ("%s\n",err?"TEST FAILED" : "TEST PASSED");
    
        /* Restore old value of INTM */
        IRQ_globalRestore(old_intm);
        
        /* We're done with MCBSP, so close it */
        MCBSP_close(mhMcbsp);                     
    }

    把代码中标记的部分注释或删除即可。