想在6678上实现与PC的组播通讯,有相应的测试例程吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
组播可以实现的,具体可以参考PDK目录下的例子
...\pdk_C6678_1_0_0_xx\packages\ti\drv\pa\test\PAUnitTest
用Pa_configExceptionRoute API增加下面的异常路由
/**
* @def pa_EROUTE_MAC_MULTICAST
* MAC multicast packet which is not specified at the lookup table
*/
#define pa_EROUTE_MAC_MULTICAST 13
/**
* @def pa_EROUTE_IP_MULTICAST
* IP multicast packet which is not specified at the lookup table
*/
#define pa_EROUTE_IP_MULTICAST 15