This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti dm368 1080i编码帧率变化的问题?



现在我的1080i 就是一个问题了,编码不稳定:        

ARM Load: 12% Video fps: 28 fps Video bit rate: 822 kbps Sound bit rate: 0 kbps
Time: 00:00:09 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolution
: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 19% Video fps: 29 fps Video bit rate: 1497 kbps Sound bit rate: 0 kbps
 Time: 00:00:10 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 16% Video fps: 23 fps Video bit rate: 1457 kbps Sound bit rate: 0 kbps
 Time: 00:00:12 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 16% Video fps: 26 fps Video bit rate: 1326 kbps Sound bit rate: 0 kbps
 Time: 00:00:13 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

fps 每秒都在变化,不知为什么?而 720p 的fps是固定在30