This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

控制台的输出问题



我用的是CCS 5.2,板子用的芯片是DM6446。使用仿真器调试如下程序:

#include <stdio.h>

 

void main(void) {

int i;

for(i = 0; i < 100; i++)

printf("%d ", i);

printf("\n");

}

控制台的输出为:
[C64XP_0] 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88[C64XP_0]  89 90 91 92 93 94 95 96 97 98 99 
我的问题是,在输出当中,CCS会插入[C64XP_0]这样的字符串(红色字体的那个),但这不是我想要的。请问如何去除这一点?