This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6747 uart 中断 求指导



 uart中断偶尔能跳转到vectors.asm,但绝大多数情况不能。请专家帮我看下到底哪里出问题了。下面是我的初始化部分
void main( void )
{
   /* 初始化6747核 */

C6747_init();
 PINMUX11 = 0x00001100;   //UART1_TXD,UART1_RintXD
CSR&=0xfffe;
asm(" NOP 2 ");
uart1=C6747_UART_OPEN(1,57600);
 INTmux1=0x2E0000;                      // 指定uart1 到中断
asm(" NOP 2 ");                      
ISTP=0x80000000;
asm(" NOP 2 ");                        // 重置中断向量表到0C00h
ICR=0xfff0;
asm(" NOP 2 ");
ISR=0x0;                            // 清除等待的中断
asm(" NOP 2 ");
IER=0xffff;
 CSR=CSR|0x1; //开总中断

UART_Handle C6747_UART_open( Uint16 id, Uint32 baudrate )
{
UART_Handle uart_handle;
Uint32 divisor;
volatile Uint16 dummy;

/*
* UART clk / baudrate
* = 150,000,000 / (900 * 16)
*/
divisor = 150000000 / ( baudrate * 16);

switch ( id )
{
case 0:
uart_handle = ( UART_Handle )&UART_MODULE_0;
break;
case 1:
uart_handle = ( UART_Handle )&UART_MODULE_1;
break;
case 2:
uart_handle = ( UART_Handle )&UART_MODULE_2;
break;
default:
return ( UART_Handle )-1;
}

uart_handle->regs->PWREMU_MGMT = 0; // Reset UART TX & RX components

C6747_wait( 100 );

uart_handle->regs->DLL = (divisor & 0xff); // Set baud rate
uart_handle->regs->DLH = (divisor >> 8);

uart_handle->regs->FCR = 0x0007; // Clear UART TX & RX FIFOs
uart_handle->regs->FCR = 0x0000; // Non-FIFO mode
uart_handle->regs->IER = 0x0007; // Enable interrupts
uart_handle->regs->LCR = 0x0003; // 8-bit words,
// 1 STOP bit generated,
// No Parity, No Stick paritiy,
// No Break control
uart_handle->regs->MCR = 0x0000; // RTS & CTS disabled,
// Loopback mode disabled,
// Autoflow disabled

uart_handle->regs->PWREMU_MGMT = 0xE001; // Enable TX & RX componenets

// Clear any pre-existing characters
dummy = uart_handle->regs->THR;
return uart_handle;
}