This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMPAL-L132 RTC问题咨询



原产品修改方案,RTC由原本外接32.768KHZ crystal修改为外接32.768KHZ频率源,RTC_CVDD由原来单独供电修改为和CPU公用VCC1V2。

RTC程序没做修改,按现在的硬件方案RTC时间不跑了。

1.已测试频率源32.768KHZ频率符合,电压幅度为0.96V.

2.RTC_CVDD已测试1.2V稳定

3.RTC程序在原硬件方案中运行正常

4.CCS5仿真测试,发现能控制CTRL寄存器BIT[0]RUN,并且STATUS寄存器BIT[1]也被置1.但时间寄存器(SENCOND,MINUTE等)一直保持复位默认值,写入后通过仿真器看寄存器second,minute等值未改变。

麻烦请教下,修改为和外部频率源和非独立供电,程序设置有需要修改吗