This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3892/DM8168 DDR3 PCB布线的问题,及原理图设计 请教

Other Parts Discussed in Thread: AM3517, DM3730

(1)我用两片16BIT的DDR3并接在AM3892下的一个片选下,参考SPRUGX7(p732页)的Figure 7-4,看不出是用AM3892的DDR_A[14:1]接到两片DDR3芯片的[A13-A0],还是用AM3892的DDR_A[13:0]接到两片DDR3芯片的[A13-A0]?

(2)此外能讲述一下DDR3的布线规则吗?  AM3892 能否 将 开发板的8片小容量 DDR3换成 两旁大容量DDR3,是否有建议参考的型号?

开发板的DDR3是菊花链拓扑布线吧,能否用2片DDR3,走类似AM3517这样的 T形拓扑?

一般来说 DDR3多片,走T行的话, 800MHz以上会有问题。 而菊花链更好。

(3). 在DDR3的布线时,需要做到等长匹配,由于DDR部分在芯片内部的走线可能存在差别,所以需要通过改变外部的走线长度来控制总的长度相等。而我在DM8168的手册里面没有看到DDR3芯片内部的走线尺寸表,所以想确认一下,AM3894 的DDR3芯片内部走线长度是否相等?
 
(4). 我阅读了之前TI的一个关于DDR3的布线指导,里面说clk信号走线的长度和address信号线的走线长度需要相等,误差在+-20mil以内。而根据我从EVM板上测得的长度来看,clk信号比address信号短,而且偏移量超出了20mil,而且控制线也比地址线短,相同组的data线之间也有最大40mil的误差,请问我到底要参照哪边?
有做DM8168或者 DM3730\AM3517 的吗?加我QQ,一起交流:我的QQ: 315676522,