This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AT25F1024自举失败



之前用的AT25256B可以自举一个几K的程序可以,但是我现在有个80多K的程序所以想用AT25F1024来自举,boot55x.cmd文件我没有变过直接去将out文件生成bin文件,然后把bin文件下载到AT25F1024中,设置GPIO 0/1/2/3 为0/1/0/0,然后就什么都没动了,因为才接触这一块所以不知道是否还需要改哪里的参数?

-e _c_int00
-boot
-v5510:2
-serial8
-reg_config 0x1c00,0x2180
-delay 0x100
-b
-o C:\exchange\codec.bin
C:\exchange\codec.out

上面是boot55x.cmd文件