This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1.6655和6671在功能上有什么区别



 6655

  http://www.ti.com.cn/cn/lit/ml/sprt629/sprt629.pdf

《Power efficient high performance DSPs for process-intensive applications》

中有以下描述

1.6655在1GHz 满载运行 功耗小于 2.5W  是否可以认为 主频下降到 800MHz 功耗6654持平。

2.6654相比6655在硬件上 少了 1M内存 和 在Hardware Accelerators 的vcp2 和TCP3d 是否占用 功耗 大概多少。

3.还有 6671的 Hardware Accelerators 为“PA” 而 6655是“vcp2 和TCP3d ”两者在性能上多大区别,在功耗上能节约多少。