This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关C6657L平台 DDR3速率的问题



大家好:

       这二天遇到的困扰:C6657L平台,仿真器SEED-XDS560V2调试,同一个gel文件(TI提供evmc6657l.gel)和程序

               1)在开发板上,gel文件初始化、加载程序、运行程序都正常;

                2)这二天做5块新的PCB(PCB是外包委托设计的)调试,说明下DDR3芯片为三星的K4B4G1646D-BCK0,其它外设只保留串口0,gel文件初始化阶段始终提示“DDR3 memory test... Failed",此处gel文件中有DDR3相关的控制器配置后,进行DDR3读写校验失败才有此提示,导致加载程序失败;接下来开始参考DDR3芯片资料进行DDR3控制器PLL和操作时序修改尝试之后,得出测试结果:

                      时钟管脚频率配置为400MHz,操作时序按DDR3-1066修改,5块板子才顺利gel文件初始化、加载程序、运行程序正常;

                     时钟管脚频率配置为533MHz,操作时序按DDR3-1066修改,只有一块板子基本gel文件初始化、加载程序、运行程序正常,其它四块板子都加载跑飞;

                     时钟管脚频率配置为533MHz,操作时序按TI提供的DDR3-1333,gel文件初始化阶段始终提示“DDR3 memory test... Failed"。

      请各位分析下问题到底出哪里?怎么有效的方法查找定位问题?

     附件中有gel文件

evmc6657l.gel