在windows环境下使用CCS编译代码通过以后生成.out文件。如何进行烧写?不太懂。没有JTAG,开发板配套的只有电源线以及数据线。应该怎么调试?
需要购买专用的JTAG线吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在windows环境下使用CCS编译代码通过以后生成.out文件。如何进行烧写?不太懂。没有JTAG,开发板配套的只有电源线以及数据线。应该怎么调试?
需要购买专用的JTAG线吗?
连接会出现错误,错误信息:
IcePick_D_0: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 6.0.14.5)
请问这个是什么问题?
IDK是用FT2232L把USB口转串口或JTAG口,请试试安装一下下面网站上的FDTI driver。
http://www.ftdichip.com/Drivers/VCP.htm