1 在C6748上测试dsplib_c674x_3_4_0_0中FFT时间,
在DSPLIB_C674x_TestReport.html中查看到DSPF_sp_fftSPxSP接口对应测试结果是:
| DSPF_sp_fftSPxSP | Passed | 1069 (N=128) 1965 (N=256) | N/A | 928 |
| Test Parameters | ||||
|---|---|---|---|---|
| Precision: | Fixed Point | |||
| Endianness: | Little | |||
| Object File Format: | COFF | |||
| Platform: | CCS Simulator | |||
| Cores Used: | 1 | |||
| CCS Version: | 5.4.0.00091 | |||
| CGT Version: | 7.4.2 | |||
我在板上实际测试时需要什么条件下才能达到这个cycle数?256点情况下;
2 在DSPF_sp_fftSPXSP的说明中有如下一段,请问是什么意思?
Interruptibility: The code is interrupt-tolerant but not interruptible.