准备在omapl138的ARM和运行linux系统,找了一个linux3_3的,每次运行的时候只运行到
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.3.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2384864 Bytes = 2.3 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel. // 运行到此处就不运行了,不知道是什么原因,请教下各位,如何解决,
如果有现成的linux,可以给我一份,谢谢