This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

自己做的C5515的板子,不小心把三个LDOI引脚给了不同的电压,两个给了1.8V,一个给了3.3V,焊板子的时候发现所有1.8V变成了3.3V,求助



各位工程师好,自己做的C5515的板子,不小心把三个LDOI引脚给了不同的电压,两个给了1.8V,一个给了3.3V,焊板子的时候发现所有1.8V变成了3.3V,请问这三个引脚内部是直接连起来的吗?重新再做板子的成本比较高,现在想用下面的方法解决。

1、焊BGA芯片前,把两个1.8V的LDO引脚的焊锡球扣掉,只让3.3V的LDOI给他们三个都供电(假设内部连起来的)

2,焊BGA芯片前,把3.3V的LDO引脚的焊锡球扣掉,让1.8V的LDOI给他们三个都供电(假设内部连起来的),这种情况可能会导致电压不够(毕竟只有1.8V)

挺急的,谢谢各位