U-Boot SPL 2016.05-00304-gad06f64-dirty (Apr 11 2017 - 16:14:05)
Core Clock:1000 MHz,Mpu Clock 800 MHz
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00304-gad06f64-dirty (Apr 11 2017 - 16:14:05 +0800)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
Watchdog enabled
DRAM: 512 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for ethernet@4a100000: addr 0
eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in SROM is de:ad:be:ef:00:01
Address in environment is b0:d5:cc:81:84:a3
, eth1: usb_ether
Press SPACE to abort autoboot in 2 seconds
=> boot
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3470488 bytes read in 308 ms (10.7 MiB/s)
38912 bytes read in 50 ms (759.8 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x34f498 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff3000, end 8ffff7ff ... OK
Starting kernel ...