This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812芯片串口烧写程序



       使用SDFlash 软件进行F2812的串口烧写,程序可以烧写进去,且提示“擦除成功、烧写成功、校验成功”。但是程序运行不对,感觉好像一直在不停的复位。总共有5种不同的程序,分别烧注到5块不同的电路板中(5种程序和电路板是一一对应的,实现5种不同的功能)。其中4个程序烧注后都能正常运行,只有1个不行。试了一下,将其他4种程序烧注到运行不对的那个电路板上,工作应该正常(由于程序和电路板不匹配,具体功能无法验证,但有个工作指示灯的闪烁是正常的);再将运行不对的程序烧注到其他4种电路板中,工作不正常(同样,由于程序和电路板不匹配,具体功能无法验证,但工作指示灯的闪烁是正常的);请问可能是什么原因?怀疑和程序有关,是不是程序操作F2812的FLASH地址和串口加载的引导程序冲突?