您好,
我这边用DM8168的USB外接USB摄像头,偶尔出错误,有的时候时候是跑很久出错,有的时候上电启动后就出错,出错后就无图像。此USB摄像头采用UVC协议,传输的分辨率为640X480/30fps,我仔细检查了供电,没有出现电压跌落。而且USB摄像头的功耗一般都不大,我在网晚上查了下,一般不到1W,所以电流应该是够的,PCB也采用了阻抗控制,PCB走线较长,但我认为传这种分辨率,速率不会太高,所以USB的信号完成性对他影响不大。如果在DM8168和USB摄像头之间串上一个USB HUB,就不会出现错误,这个HUB我没有提供外部电源。还请帮忙分析下,是软件驱动问题还是硬件问题,具体是怎么回事,出错的打印信息如下:
ti81xx_interrupt 960: CAUTION: musb1: Babble Interrupt Occured
ti81xx_interrupt 961: Please issue long reset to make usb functional !!
ti81xx_interrupt 1059: Babble: devtcl(90)Restarting musb....
evm_deferred_musb_restart 895: deferred musb restart musbid(1)
usb 2-1: USB disconnect, address 35
Fail to ioctl 'VIDIOC_STREAMOFF': No such device
谢谢!