This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

官网原理图设计是否能满足RTC_PWRONRSTn复位至少1ms?



大家好:

AM335X PDF上说RTC_PWRONRSTn复位至少保证1ms。

TMDSSK3358_3H0009_REV1_2B_SCH原理图RTC复位是与门和RC处理的,R=1K  C=0.01uF,这个RC延时算下来远远小于1MS。这个复位能满足吗?

另外,R125 100K到地有什么作用?

  • 这个设计没什么问题,是验证过的。

    100K应该是个弱下拉设计。

  • 非常感谢您的答复!

    我们的产品发现有几例是上电时PMIC_POWER_EN没有输出高电平(VDDS_RTC=1.8V)。我是这样理解的:PMIC_POWER_EN输出高电平有两个条件VDDS_RTC先输出1.8V高电平同时RTC_PWRONRSTn 为低电平。我原设计直接将RTC_PWRONRSTn用100K拉高到1.8V,开始以为是没加RC延时的原因,不过加过至少1MS延时(R=10K , C=0.1uf)后,还是有这个现象。我的设计与官网开发板对比后,发现这部分设计就差这个两个与门了。这里与门有什么呢?