This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教ezdsp5535的USB连接问题



各位专家,我在ezDSP5535开发板上用CCS5.3,运行c55_csl_304\ccs_v50_examples\usb\CSL_USB_DmaExample,昨晚之前的USB连接都正常,但从昨晚开始调试过程中发现运行程序后USB连接不上,程序卡在csl_usb_dma_example.c中的下面这一句处

while(CSL_FEXT(usbRegisters->DEVCTL, USB_DEVCTL_VBUS) != CSL_USB_DEVCTL_VBUS_ABOVEVBUSVALID); //wait vbus insert

今天上午换了一个USB口后能连接上了(但我没有再去测之前的USB口能否连接),但下午后来的USB口也连不上了,现象同上。电脑的两个USB口都可以正常连接U盘和XDS100V2,观察DEVCTL寄存器内容为0x0000,测试开发板上的VBUS测试点为4.8V,请问会不会5535的VBUS引脚虚焊?还有可能是其他什么原因?

谢谢!