This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6748执行时间的问题



程序结构如下

void main(void)

{    init();

    while(1)

{  printf("c");

    myfunction();

}

以上程序在C6748 400MHz DSP上运行 。通过TSC定时器测试发现 执行一次while 需要18ms 。但是硬件串口每秒只收到了  12个字符 "c"  按理应收到1000/18=55个"c"  才是正确的啊。  串口波特率设置为57600bps。这是什么原因呢。