项目要求DSP不跑操作系统,arm核上linux3.3,在做双核通信的linux设备驱动时候遇到了一个诡异的问题,只要DSP通过CHIPSIG_INT0触发ARM中断,ARM中的linux内核的其他很多驱动都停止了工作,连自己的led控制驱动都失去了响应,流水灯也失去了闪烁,LCD显示也停止了刷新,但是运行GUI还是可以显示界面,就是界面不能刷新,触摸屏也不懂了。好像是其他驱动都阻塞了!!!!
我的linux设备驱动是这样实现的:使用Tasklet实现软中断,只要DSP的数据一准备好就通过CHIPSIG_INT0触发ARM中断,这时候驱动的tasklet顶半部会立刻响应中断去读取数据,然后调度tasklet的底半部,这样的流程一般是没问题才对,但是现象就是只要顶半部被触发了,其他驱动就异常了,linux也没有任何提示,而且无法恢复,触发重启内核,但是唯独这个驱动完全正常运行,数据照样读取也不丢帧,而且奇怪的事,DSP触发CHIPSIG_INT0,ARM核会触发两次两次中断,我的驱动实现如下,麻烦帮忙看下。
#include<linux/init.h>
#include<linux/module.h>
#include<linux/kernel.h>
#include<linux/fs.h>
#include<linux/types.h>
#include<linux/ioctl.h>
#include<linux/cdev.h>
#include<linux/kdev_t.h>
#include<mach/hardware.h>
#include<linux/gpio.h>
#include <asm/mach-types.h>
#include <asm/mach/arch.h>
#include <mach/da8xx.h>
#include <mach/mux.h>
#include <mach/irqs.h>
#include <linux/interrupt.h>
#include "k_linkQueue.h"
#include "memory_map.h"
#include <linux/wait.h>//for 等待队列api
#include <linux/errno.h>
//引入其他模块函数和变量
extern Ping_Pong_Buffer res_buff;
extern char k_linkQueue_create(linkQueue *queue, unsigned int dataType, unsigned int blockNumber, unsigned int blockSize);//创建链队列
extern void k_linkQueue_release(linkQueue *queue);//释放链队列
extern unsigned int k_linkQueue_insertData(linkQueue *queue, void *data, int force);//链队列插入数据
extern unsigned int k_linkQueue_getData(linkQueue *queue, void *r_buff);//获取队列的数据
extern void SHM_ARM_Init(unsigned char* const mem_base);//共享内存初始化
static int read_quest = 0;//如果有读取数据请求且链队列无数据可读,则置1
//设置主从设备号
#define PROTOCOL_MAJOR 1
#define PROTOCOL_MINOR 0
//定义设备驱动的名字或设备节点的名字
#define DEVICE_NAME "protocol_driver"
//定义全局的循环队列作为数据缓冲区
k_linkQueue queue;
//寄存器地址映射全局变量
unsigned int *R_CHIPSIG = NULL;//CHIPSIG寄存器
unsigned int *R_CHIPSIG_CLR = NULL;//CHIPSIG_CLR寄存器
//物理内存映射全局变量
volatile void *mem_base = NULL;
volatile unsigned char *cur_buf_ptr = NULL;
volatile unsigned char *data_ready_ptr = NULL;
//定义读数据等待队列头,IO阻塞
DECLARE_WAIT_QUEUE_HEAD(wait_queue_head);
//定义原子变量
static atomic_t dev_available = ATOMIC_INIT(1);//原子变量的值为1,即只能一个进程打开此设备
//定义设备类
static struct class *protocol_class;
struct cdev *protocol_cdev;
dev_t protocol_dev_no;
/*定义tasklet和声明底半部函数并关联*/
void read_data_tasklet(unsigned long);
DECLARE_TASKLET(CHIPINT0_tasklet,read_data,0);
//将CHIPINT0_tasklet与read_data绑定,传入参数0
/*中断处理底半部, 拷贝内存*/
void read_data(unsigned long a)
{
if(read_quest == 1)//如果进程调用了此驱动的read函数且链队列没有数据可读,read_quest将会被赋值为1
{
read_quest = 0;
//通过底半部唤醒被阻塞的读取进程
wake_up_interruptible(&wait_queue_head);//唤醒读等待队列
}
}
/*中断处理顶半部*/
irqreturn_t CHIPINT0_interrupt(int irq,void *dev_id)
{
//只要一触发进入这个程序,其他驱动会出问题,即使这个程序什么都不做也会这样
volatile Buffer_Type *next_read;
//如果DSP数据已经ready
if(*(res_buff.cur_buffer->data_ready) == 1)//DSP触发一次中断,ARM会进入此中断两次!!,因此用ready标识防止节奏混乱
{
if(*(res_buff.bufferID_ptr) == BUFF_ID_PING)//切换读buffer
{
next_read = &res_buff.pong_buffer;//下一次中断读pong buffer
//printk(KERN_ALERT"read ping\n");
}
else
{
next_read = &res_buff.ping_buffer;//下一次中断读ping buffer
//printk(KERN_ALERT"read pong\n");
}
*(res_buff.bufferID_ptr) ^= BUFF_ID_PING;//切换DSP写另一个buffer
//将数据插入链队列
k_linkQueue_insertData(&queue, res_buff.cur_buffer->buf_ptr, 0);
//标识位都重置
*(res_buff.cur_buffer->data_ready) = 0;
*(res_buff.cur_buffer->data_size) = 0;
res_buff.cur_buffer = next_read;
}
//清楚中断标识
*R_CHIPSIG_CLR = 1 << 0;//clear chipint0 status
tasklet_schedule(&CHIPINT0_tasklet);//调度底半部
return IRQ_HANDLED;
}
//文件打开函数
static int protocol_open(struct inode *inode, struct file *file)
{
int result = 0;
if(!atomic_dec_and_test(&dev_available))
{
atomic_inc(&dev_available);
return -EBUSY;//设备已经被打开
}
printk (KERN_ALERT "\nprotrol driver open\n");
return 0;
}
//文件释放函数
static int protocol_release(struct inode *inode, struct file *filp)
{
atomic_inc(&dev_available);//释放设备,原子变量加1
printk (KERN_ALERT "device released\n");
return 0;
}
//文件读函数
static int protocol_read(struct file *filp, char *dst, size_t size, loff_t*offset)
{
int ret = 0;
//定义等待队列
DECLARE_WAITQUEUE(wait_queue, current);//定义等待队列
add_wait_queue(&wait_queue_head, &wait_queue);//添加等待队列
if(queue.remainNumber == queue.blockNumber)//当前buffer没数据
{
//printk(KERN_ALERT"\nbuffer no data\n");
//如果是非阻塞方式读取,则直接跳出
if(filp->f_flags & O_NONBLOCK)
{
ret = -EAGAIN;
goto out;
}
//阻塞当前进程,放弃cpu资源
read_quest = 1;
__set_current_state(TASK_INTERRUPTIBLE);//改变进程状态为睡眠
schedule();//调度其他进程运行
if(signal_pending(current))
{
//如果是因为信号被唤醒,则返回到系统调用之前的地方
ret = -ERESTARTSYS;
goto out;
}
}
//将数据拷贝到用户空间
ret = k_linkQueue_getData(&queue, dst);
if(ret == 0)
{
//printk(KERN_ALERT"\ncopy data to user space failed :%d\n", ret);
}
out:
remove_wait_queue(&wait_queue_head, &wait_queue);//移除等待队列
set_current_state(TASK_RUNNING);//设置当前进程为运行状态
return ret;
}
static long protocol_ioctl(struct file *file, unsigned int cmd, unsigned long value)
{
return 0;
}
/*驱动文件操作结构体,file_operations结构体中的成员函数会在应用程序进行
open()、release()、ioctl()协同调用时被调用*/
static const struct file_operations protocol_fops =
{
.owner = THIS_MODULE,
.open = protocol_open,
.release = protocol_release,
.read = protocol_read,
// .write = protocol_write,
.unlocked_ioctl=protocol_ioctl,
};
/*设备驱动模块加载函数*/
int __init protocol_init(void)
{
int ret = 0;
int result = 0;
//申请注册设备号(动态)
ret=alloc_chrdev_region(&protocol_dev_no, PROTOCOL_MINOR, 1, DEVICE_NAME);
if(ret < 0)
{
printk(KERN_EMERG "alloc_chrdev_region failed\n");
return 0;
}
//分配cdev
protocol_cdev = cdev_alloc();
if(protocol_cdev == NULL)
{
printk(KERN_EMERG "Cannot alloc cdev\n");
return 0;
}
//初始化cdev
cdev_init(protocol_cdev,&protocol_fops);
protocol_cdev->owner=THIS_MODULE;
//注册cdev
cdev_add(protocol_cdev, protocol_dev_no, 1);
//创建一个类
protocol_class = class_create(THIS_MODULE, DEVICE_NAME);
//创建设备节点
device_create(protocol_class, NULL, protocol_dev_no, NULL, DEVICE_NAME);
//申请链式循环队列作为缓冲区DSP数据帧的缓冲区
k_linkQueue_create(&queue, sizeof(double), 1000, DATA_BLOCK_SIZE);//申请1000个blocksize的队列空间作为帧缓冲区
//映射ARM的核间通讯寄存器
R_CHIPSIG = ioremap(SOC_SYSCFG_0_REGS + SYSCFG0_CHIPSIG, 4);
R_CHIPSIG_CLR = ioremap(SOC_SYSCFG_0_REGS + SYSCFG0_CHIPSIG_CLR, 4);
//将物理地址映射到内核空间
mem_base = ioremap(SHARED_BUFFER_ADDR, SHARED_BUFFER_SIZE);
//共享内存初始化
SHM_ARM_Init((unsigned char *)mem_base);
/*申请中断*/
/*
参数说明:
IRQ_DA8XX_CHIPINT0:要申请的中断号
CHIPINT0_interrupt:向内核登记的中断处理程序(顶半部),为一个回调
IRQF_DISABLED:表明中断处理程序是快速处理程序,快速处理程序被调用时屏蔽所有中断
"DSP Signal":名称
NULL:在中断共享时会用到,这里设置为NULL
*/
result = request_irq(IRQ_DA8XX_CHIPINT0, CHIPINT0_interrupt,IRQF_SHARED,"DSP Signal",&protocol_cdev);
if(result != 0)
{
if(result == -EINVAL)
{
printk(KERN_ALERT "irq request err:-EINVAL\n");
}
else if(result == -EBUSY)
{
printk(KERN_ALERT "irq request err:--EBUSY\n");
}
else
{
printk(KERN_ALERT "irq request err: unknown\n");
}
return result;
}
return 0;
}
/*设备驱动模块卸载函数*/
void __exit protocol_exit(void)
{
/*释放中断*/
/*
参数详解:
IRQ_DA8XX_CHIPINT0:中断号
NULL:void *dev_id,这个参数是中断共享的时候用到的,此驱动不共享中断,因此为NULL
*/
free_irq(IRQ_DA8XX_CHIPINT0, NULL);
//释放帧缓冲的内存
k_linkQueue_release(&queue);
//释放寄存器映射
iounmap(R_CHIPSIG);
iounmap(R_CHIPSIG_CLR);
cdev_del(protocol_cdev); //删除cdev
unregister_chrdev_region(protocol_dev_no, 1); //注销设备号
device_destroy(protocol_class, protocol_dev_no); //销毁设备节点
class_destroy(protocol_class); //销毁设备类
printk(KERN_ALERT "exit success\n");
}
//驱动被加载或被卸载自动执行的函数
module_init(protocol_init);
module_exit(protocol_exit);
MODULE_LICENSE("GPL");
MODULE_VERSION ("v0.9");
MODULE_AUTHOR("None");
MODULE_DESCRIPTION("driver");