This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个电压默认输出应该是1.1V,看看是不是外部电感电容焊错了。
电源输出有时对了,但是要VBAT重新上电,EXP_PWR_ON开关多次配合复位情况下,vdd_mpu=1.1V,有时不对,有时能正常。估计是RTC_PROZ时间不对,但是这个图是按照TI demo 来的啊。
请问你是参考哪个demo板的原理图做的设计?RTC_PORZ和这个VDD_MPU没有关系。
参考的TMDSSK3358 Board,为什么有时候启动不了,vdd_mpu不对。
参考TMDSSK3358 的电源TPS65910A3A1电路,通过外部EX_PB_POWERON 按键长时间接地松开,不是每次VDD_MPU 1.1V,有时是0.46左右?何解?