This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359 EVM 板从nand启动的问题

Other Parts Discussed in Thread: TPS65910, AM3359

我用的官方的BSP。但是在kernel下nand没有驱动起来,求大师指点。谁在nand下成功挂载文件系统并启动的....(ramdisk除外)。

  • 你用的什么办法烧写的nand?起不来,值得是哪一步起不来,能具体说说么

  • root@am335x-evm:~# dmesg
    [    0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.3.3 (GCC) ) #3 S
    un Sep 2 01:57:55 PDT 2012
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
    n cache
    [    0.000000] Machine: am335xevm
    [    0.000000] Memory policy: ECC disabled, Data cache writeback
    [    0.000000] On node 0 totalpages: 65536
    [    0.000000] free_area_init_node: node 0, pgdat c0613374, node_mem_map c064900
    0
    [    0.000000]   Normal zone: 512 pages used for memmap
    [    0.000000]   Normal zone: 0 pages reserved
    [    0.000000]   Normal zone: 65024 pages, LIFO batch:15
    [    0.000000] AM335X ES1.0 (sgx neon )
    [    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
    [    0.000000] pcpu-alloc: [0] 0
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pag
    es: 65024
    [    0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait console=ttyO0,1
    15200
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 256MB = 256MB total
    [    0.000000] Memory: 253420k/253420k available, 8724k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc0580000   (5600 kB)
    [    0.000000]       .init : 0xc0580000 - 0xc05bf000   ( 252 kB)
    [    0.000000]       .data : 0xc05c0000 - 0xc061c088   ( 369 kB)
    [    0.000000]        .bss : 0xc061c0ac - 0xc0648d30   ( 180 kB)
    [    0.000000] NR_IRQS:396
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
    ts
    [    0.000000] Total of 128 interrupts on 1 active controller
    [    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
    [    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
    [    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13
    1071999ms
    [    0.000000] Console: colour dummy device 80x30
    [    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
    [    0.058532] pid_max: default: 32768 minimum: 301
    [    0.058654] Security Framework initialized
    [    0.058776] Mount-cache hash table entries: 512
    [    0.059143] CPU: Testing write buffer coherency: ok
    [    0.079162] omap_hwmod: gfx: failed to hardreset
    [    0.095428] omap_hwmod: pruss: failed to hardreset
    [    0.096588] print_constraints: dummy:
    [    0.096954] NET: Registered protocol family 16
    [    0.099243] OMAP GPIO hardware version 0.1
    [    0.101928] omap_mux_init: Add partition: #1: core, flags: 0
    [    0.104217]  omap_i2c.1: alias fck already exists
    [    0.105163]  omap2_mcspi.1: alias fck already exists
    [    0.105407]  omap2_mcspi.2: alias fck already exists
    [    0.105682]  edma.0: alias fck already exists
    [    0.105682]  edma.0: alias fck already exists
    [    0.105712]  edma.0: alias fck already exists
    [    0.131378] bio: create slab <bio-0> at 0
    [    0.133636] SCSI subsystem initialized
    [    0.135345] usbcore: registered new interface driver usbfs
    [    0.135650] usbcore: registered new interface driver hub
    [    0.135864] usbcore: registered new device driver usb
    [    0.136016] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
    [    0.136322] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
    [    0.148620] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
    [    0.150482] tps65910 1-002d: JTAGREVNUM 0x0
    [    0.152893] print_constraints: VRTC:
    [    0.154357] print_constraints: VIO: at 1800 mV
    [    0.156677] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
    [    0.158996] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
    [    0.160034] print_constraints: VDD3: 5000 mV
    [    0.161437] print_constraints: VDIG1: at 1800 mV
    [    0.162872] print_constraints: VDIG2: at 1800 mV
    [    0.164306] print_constraints: VPLL: at 1800 mV
    [    0.165740] print_constraints: VDAC: at 1800 mV
    [    0.167175] print_constraints: VAUX1: at 1800 mV
    [    0.168609] print_constraints: VAUX2: at 3300 mV
    [    0.170043] print_constraints: VAUX33: at 3300 mV
    [    0.171478] print_constraints: VMMC: at 3300 mV
    [    0.171997] tps65910 1-002d: No interrupt support, no core IRQ
    [    0.172943] Advanced Linux Sound Architecture Driver Version 1.0.24.
    [    0.174102] Switching to clocksource gp timer
    [    0.190185] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
    [    0.190368] musb-hdrc musb-hdrc.0: dma type: pio
    [    0.190704] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk
     split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    [    0.190734] musb-hdrc: MHDRC RTL version 2.0
    [    0.190734] musb-hdrc: setup fifo_mode 4
    [    0.190765] musb-hdrc: 28/31 max ep, 16384/16384 memory
    [    0.191253] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using
    PIO, IRQ 18
    [    0.191406] musb-hdrc musb-hdrc.1: dma type: pio
    [    0.191711] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk
     split, HB-ISO Rx, HB-ISO Tx, SoftConn)
    [    0.191741] musb-hdrc: MHDRC RTL version 2.0
    [    0.191772] musb-hdrc: setup fifo_mode 4
    [    0.191802] musb-hdrc: 28/31 max ep, 16384/16384 memory
    [    0.191833] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    [    0.191894] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
    r 1
    [    0.192047] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    0.192077] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
    1
    [    0.192077] usb usb1: Product: MUSB HDRC host driver
    [    0.192108] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
    [    0.192108] usb usb1: SerialNumber: musb-hdrc.1
    [    0.192901] hub 1-0:1.0: USB hub found
    [    0.192932] hub 1-0:1.0: 1 port detected
    [    0.193481] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using
     PIO, IRQ 19
    [    0.193908] NET: Registered protocol family 2
    [    0.194091] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.194519] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.194671] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.194763] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.194793] TCP reno registered
    [    0.194793] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.194824] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.195007] NET: Registered protocol family 1
    [    0.195281] RPC: Registered named UNIX socket transport module.
    [    0.195281] RPC: Registered udp transport module.
    [    0.195312] RPC: Registered tcp transport module.
    [    0.195312] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.195587] NetWinder Floating Point Emulator V0.97 (double precision)
    [    0.207824] VFS: Disk quotas dquot_6.5.2
    [    0.207885] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.208435] msgmni has been set to 494
    [    0.209228] io scheduler noop registered
    [    0.209228] io scheduler deadline registered
    [    0.209289] io scheduler cfq registered (default)
    [    0.210632] Could not set LED4 to fully on
    [    0.212432] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
    [    0.816650] console [ttyO0] enabled
    [    0.820922] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [    0.828796] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [    0.836608] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    [    0.844390] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    [    0.852172] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    [    0.869537] brd: module loaded
    [    0.877716] loop: module loaded
    [    0.881195] i2c-core: driver [tsl2550] using legacy suspend method
    [    0.887695] i2c-core: driver [tsl2550] using legacy resume method
    [    0.894104] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [    0.954681] No daughter card found
    [    0.958282] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
    [    0.973449] AM335X: wrong header 0xffffffff, expected 0xee3355aa
    [    0.979888] The board is windycore EVM in profile 0
    [    0.984985] ===============windycore=========================
    [    0.990966] Found invalid GP EVM revision, falling back to Rev1.1A
    [    0.997650]  omap_hsmmc.0: alias fck already exists
    [    1.003417]  omap_hsmmc.2: alias fck already exists
    [    1.008911] Configure Bluetooth Enable pin...
    [    1.015747] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    1.022888] omap2-nand driver initializing
    [    1.028533] CAN device driver interface
    [    1.032562] CAN bus driver for Bosch D_CAN controller 1.0
    [    1.084808] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    [    1.091278] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    [    1.098571] davinci_mdio.0: probed
    [    1.102142] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
    [    1.109863] usbcore: registered new interface driver zd1201
    [    1.115905] usbcore: registered new interface driver cdc_ether
    [    1.122131] usbcore: registered new interface driver cdc_eem
    [    1.128234] usbcore: registered new interface driver dm9601
    [    1.134094] cdc_ncm: 04-Aug-2011
    [    1.137634] usbcore: registered new interface driver cdc_ncm
    [    1.143554] Initializing USB Mass Storage driver...
    [    1.148864] usbcore: registered new interface driver usb-storage
    [    1.155151] USB Mass Storage support registered.
    [    1.160430] mousedev: PS/2 mouse device common for all mice
    [    1.167388] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    [    1.174041] omap_rtc: already running
    [    1.178100] i2c /dev entries driver
    [    1.182128] Linux video capture interface: v2.00
    [    1.187316] usbcore: registered new interface driver uvcvideo
    [    1.193328] USB Video Class driver (1.1.1)
    [    1.199645] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [    1.208282] cpuidle: using governor ladder
    [    1.213073] cpuidle: using governor menu
    [    1.223083] usbcore: registered new interface driver usbhid
    [    1.228942] usbhid: USB HID core driver
    [    1.233551] usbcore: registered new interface driver snd-usb-audio
    [    1.241912] ALSA device list:
    [    1.245056]   No soundcards found.
    [    1.248596] oprofile: hardware counters not available
    [    1.253875] oprofile: using timer interrupt.
    [    1.258361] nf_conntrack version 0.5.0 (3959 buckets, 15836 max)
    [    1.265136] ip_tables: (C) 2000-2006 Netfilter Core Team
    [    1.270812] TCP cubic registered
    [    1.274200] NET: Registered protocol family 17
    [    1.278869] can: controller area network core (rev 20090105 abi 8)
    [    1.285400] NET: Registered protocol family 29
    [    1.290039] can: raw protocol (rev 20090105)
    [    1.294494] can: broadcast manager protocol (rev 20090105 t)
    [    1.300476] Registering the dns_resolver key type
    [    1.305450] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
     rev 3
    [    1.313476] ThumbEE CPU extension supported.
    [    1.317993] mux: Failed to setup hwmod io irq -22
    [    1.323577] Power Management for AM33XX family
    [    1.328460] Trying to load am335x-pm-firmware.bin (60 secs timeout)
    [    1.335144] Copied the M3 firmware to UMEM
    [    1.339416] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not su
    pport st_shift
    [    1.351928] clock: disabling unused clocks to save power
    [    1.359710] Detected MACID=0:18:31:e3:8:88
    [    1.365478] omap_rtc omap_rtc: setting system clock to 2012-04-11 10:22:23 UT
    C (1334139743)
    [    1.374816] Waiting for root device /dev/mmcblk0p2...
    [    1.417724] mmc0: new high speed SDHC card at address 1234
    [    1.424102] mmcblk0: mmc0:1234 SA04G 3.63 GiB
    [    1.431152]  mmcblk0: p1 p2 p3
    [    9.062103] kjournald starting.  Commit interval 5 seconds
    [    9.067962] EXT3-fs (mmcblk0p2): warning: maximal mount count reached, runnin
    g e2fsck is recommended
    [    9.761108] EXT3-fs (mmcblk0p2): using internal journal
    [    9.766601] EXT3-fs (mmcblk0p2): recovery complete
    [    9.775482] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
    [    9.782745] VFS: Mounted root (ext3 filesystem) on device 179:2.
    [    9.789398] Freeing init memory: 252K
    [   10.290100] udevd (625): /proc/625/oom_adj is deprecated, please use /proc/62
    5/oom_score_adj instead.
    [   13.705230] kjournald starting.  Commit interval 5 seconds
    [   13.711120] EXT3-fs (mmcblk0p3): warning: maximal mount count reached, runnin
    g e2fsck is recommended
    [   14.458404] EXT3-fs (mmcblk0p3): using internal journal
    [   14.463867] EXT3-fs (mmcblk0p3): recovery complete
    [   14.468902] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode
    [   14.543487] alignment: ignoring faults is unsafe on this CPU.  Defaulting to
    fixup mode.
    [   24.234497]
    [   24.234497] CPSW phy found : id is : 0x4dd074
    [   24.241455] PHY 0:01 not found
    [   27.226196] PHY: 0:00 - Link is Up - 100/Full
    [   40.637054]  gadget: Mass Storage Function, version: 2009/09/11
    [   40.643280]  gadget: Number of LUNs=2
    [   40.647186]  lun0: LUN: removable file: /dev/mmcblk0p1
    [   40.652526]  lun1: LUN: removable file: /dev/mmcblk0p3
    [   40.657958]  gadget: Mass Storage Gadget, version: 2009/09/11
    [   40.663940]  gadget: userspace failed to provide iSerialNumber
    [   40.670074]  gadget: g_mass_storage ready
    [   40.674285] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    [   40.679870] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus numbe
    r 2
    [   40.687744] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    [   40.694824] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=
    1
    [   40.702392] usb usb2: Product: MUSB HDRC host driver
    [   40.707733] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
    [   40.713287] usb usb2: SerialNumber: musb-hdrc.0
    [   40.718627] hub 2-0:1.0: USB hub found
    [   40.722595] hub 2-0:1.0: 1 port detected
    [   87.127746] nand: exports duplicate symbol nand_default_bbt (owned by kernel)

    root@am335x-evm:~#

     

     

     

    这是我的dmesg,没有关于nand初始化的信息,我在启动之后cat /proc/mtd也捕捉不到设备,menuconfig里面该选的都选了,而且就是官方的config。

  • 你是用的SD卡启动,然后在linux里查看nand 信息,对么? 那么你看看uboot起来的时候的log,是否提示有nand?

  • 呵呵,uboot下nand可以看的到的,我也用从nand启动过uboot,这没问题。

    现在主要还是kernel阶段nand驱动不起来。

  • nand flash的驱动打开了么,有没有根据你选的flash做配置。

  • WPI的板子,我看了下原理图PCB,和TI的EVM一样。元器件也没有更换。

    目前我用了一个新的内核在尝试,这个内核我朋友那边已经驱动起nand了。我这边跑到一半就停下来了。具体信息如下

    U-Boot SPL 2011.09 (May 02 2012 - 20:17:18)

    Texas Instruments Revision detection unimplemented

    OMAP SD/MMC: 0

    reading u-boot.img

    reading u-boot.img

    U-Boot 2011.09 (Apr 17 2012 - 19:19:12)

    I2C:   ready

    DRAM:  256 MiB

    WARNING: Caches not enabled

    No daughter card present

    NAND:  HW ECC Hamming Code selected

    256 MiB

    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1

    *** Warning - bad CRC, using default environment

    Net:   cpsw

    Hit any key to stop autoboot:  0

    SD/MMC found on device 0

    reading uEnv.txt

    ** Unable to read "uEnv.txt" from mmc 0:1 **

    reading uImage

    3061680 bytes read

    ## Booting kernel from Legacy Image at 80007fc0 ...

      Image Name:   Linux-3.2.0

      Image Type:   ARM Linux Kernel Image (uncompressed)

      Data Size:    3061616 Bytes = 2.9 MiB

      Load Address: 80008000

      Entry Point:  80008000

      Verifying Checksum ... OK

      XIP Kernel Image ... OK

    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.

    [    0.000000] Linux version 3.2.0 (jack@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #2 Sun May 13 17:50:32 PDT 2012

    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d

    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

    [    0.000000] Machine: am335xevm

    [    0.000000] Memory policy: ECC disabled, Data cache writeback

    [    0.000000] AM335X ES1.0 (sgx neon )

    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024

    [    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none

    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)

    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

    [    0.000000] Memory: 256MB = 256MB total

    [    0.000000] Memory: 253468k/253468k available, 8676k reserved, 0K highmem

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    [    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)

    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)

    [    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)

    [    0.000000]       .text : 0xc0008000 - 0xc0575000   (5556 kB)

    [    0.000000]       .init : 0xc0575000 - 0xc05b2000   ( 244 kB)

    [    0.000000]       .data : 0xc05b2000 - 0xc060fb58   ( 375 kB)

    [    0.000000]        .bss : 0xc060fb7c - 0xc063c824   ( 180 kB)

    [    0.000000] NR_IRQS:396

    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts

    [    0.000000] Total of 128 interrupts on 1 active controller

    [    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz

    [    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz

    [    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms

    [    0.000000] Console: colour dummy device 80x30

    [    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)

    [    0.058929] pid_max: default: 32768 minimum: 301

    [    0.059051] Security Framework initialized

    [    0.059173] Mount-cache hash table entries: 512

    [    0.059539] CPU: Testing write buffer coherency: ok

    [    0.079528] omap_hwmod: gfx: failed to hardreset

    [    0.095794] omap_hwmod: pruss: failed to hardreset

    [    0.096893] print_constraints: dummy:

    [    0.097259] NET: Registered protocol family 16

    [    0.099426] OMAP GPIO hardware version 0.1

    [    0.102050] omap_mux_init: Add partition: #1: core, flags: 0

    [    0.104217]  omap_i2c.1: alias fck already exists

    [    0.105133]  omap2_mcspi.1: alias fck already exists

    [    0.105346]  omap2_mcspi.2: alias fck already exists

    [    0.105590]  edma.0: alias fck already exists

    [    0.105621]  edma.0: alias fck already exists

    [    0.105621]  edma.0: alias fck already exists

    [    0.130371] bio: create slab <bio-0> at 0

    [    0.132537] SCSI subsystem initialized

    [    0.134185] usbcore: registered new interface driver usbfs

    [    0.134490] usbcore: registered new interface driver hub

    [    0.134704] usbcore: registered new device driver usb

    [    0.134857] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3

    [    0.135131] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1

    [    0.136260] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz

    [    0.138122] tps65910 1-002d: JTAGREVNUM 0x0

    [    0.140533] print_constraints: VRTC:

    [    0.141998] print_constraints: VIO: at 1800 mV

    [    0.144317] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal

    [    0.146606] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal

    [    0.147613] print_constraints: VDD3: 5000 mV

    [    0.149017] print_constraints: VDIG1: at 1800 mV

    [    0.150451] print_constraints: VDIG2: at 1800 mV

    [    0.151855] print_constraints: VPLL: at 1800 mV

    [    0.153289] print_constraints: VDAC: at 1800 mV

    [    0.154693] print_constraints: VAUX1: at 1800 mV

    [    0.156158] print_constraints: VAUX2: at 3300 mV

    [    0.157562] print_constraints: VAUX33: at 3300 mV

    [    0.158996] print_constraints: VMMC: at 3300 mV

    [    0.159484] tps65910 1-002d: No interrupt support, no core IRQ

    [    0.160400] Advanced Linux Sound Architecture Driver Version 1.0.24.

    [    0.161529] Switching to clocksource gp timer

    [    0.177124] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)

    [    0.177276] musb-hdrc musb-hdrc.0: dma type: pio

    [    0.178161] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using PIO, IRQ 18

    [    0.178314] musb-hdrc musb-hdrc.1: dma type: pio

    [    0.178710] musb-hdrc musb-hdrc.1: MUSB HDRC host driver

    [    0.178802] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1

    [    0.178924] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

    [    0.178924] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    [    0.178955] usb usb1: Product: MUSB HDRC host driver

    [    0.178955] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd

    [    0.178985] usb usb1: SerialNumber: musb-hdrc.1

    [    0.179779] hub 1-0:1.0: USB hub found

    [    0.179809] hub 1-0:1.0: 1 port detected

    [    0.180328] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using PIO, IRQ 19

    [    0.180755] NET: Registered protocol family 2

    [    0.180969] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

    [    0.181274] TCP established hash table entries: 8192 (order: 4, 65536 bytes)

    [    0.181427] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

    [    0.181518] TCP: Hash tables configured (established 8192 bind 8192)

    [    0.181549] TCP reno registered

    [    0.181549] UDP hash table entries: 256 (order: 0, 4096 bytes)

    [    0.181640] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

    [    0.181823] NET: Registered protocol family 1

    [    0.182098] RPC: Registered named UNIX socket transport module.

    [    0.182128] RPC: Registered udp transport module.

    [    0.182128] RPC: Registered tcp transport module.

    [    0.182128] RPC: Registered tcp NFSv4.1 backchannel transport module.

    [    0.182403] NetWinder Floating Point Emulator V0.97 (double precision)

    [    0.194519] VFS: Disk quotas dquot_6.5.2

    [    0.194610] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

    [    0.195129] msgmni has been set to 495

    [    0.195922] io scheduler noop registered

    [    0.195953] io scheduler deadline registered

    [    0.196014] io scheduler cfq registered (default)

    [    0.197296] Could not set LED4 to fully on

    [    0.199035] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0

    [    0.807800] console [ttyO0] enabled

    [    0.812072] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1

    [    0.819915] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2

    [    0.827728] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3

    [    0.835510] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4

    [    0.843292] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5

    [    0.860412] brd: module loaded

    [    0.868530] loop: module loaded

    [    0.872009] i2c-core: driver [tsl2550] using legacy suspend method

    [    0.878509] i2c-core: driver [tsl2550] using legacy resume method

    [    0.884918] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write

    [    0.952087] No daughter card found

    [    0.955688] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write

    [    0.968811] AM335X: wrong header 0xffffffff, expected 0xee3355aa

    [    0.975097] The error message above indicates that there is an issue with

    [    0.975097] the EEPROM or the EEPROM contents.  After verifying the EEPROM

    [    0.975097] contents, if any, refer to the am335x_evm_setup function in the

    [    0.975128] arch/arm/mach-omap2/board-am335xevm.c file to modify the board

    [    0.975128] initialization code to match the hardware configuration

    到这里就不动了。

  • 你用的kernel是wt提供的,还是直接用的ti发布的?

  • 都用过,都能起来。就是nand没起来。WPI提供的也是官方的SDK包。

  • 建议你直接用wpi的sdk包,看看,如果起不来下,先问问他们。我这边的确不知道他们做了什么修改,我怀疑还是配置的问题。

  • 附件是WPI修改之后的board.c

  • 我建议你直接跟wpi的人联系下吧,你买了他们的板子,他们应该给你正确的sdk启动板子,我这边没有他们的板子,原理图,仅仅通过board 文件,一下子也找不到问题在哪里

  • 他们研发说nand还没做好...额...

  • 好吧, 你也可以自己试试调试nand flash

  • 嗯,正在用打印调试,发现他们的驱动完全没有初始化nand,估计要搞好几天了。

  • 调好了,写个调试过程上来,可以得奖的,哈哈

  • 上次参加TI研讨会,那个礼仪小姐真心漂亮,我拿驱动换媳妇儿。

  • 好吧,我相信你可以

  • 您好  我裁减了AM3359的 EVM板子只保留了baseboard上的sd 串口 usb,去掉了daughterborad。然后用sd启动系统,起不起来了。卡在了这里:Waiting for root device /dev/mmcblk0p2...

    下面是启动信息:

    请问是什么原因呢?找了好久已然没有解决。急死了

    U-Boot SPL 2011.09 (Feb 09 2012 - 15:38:59)

    Texas Instruments Revision detection unimplemented

    Could not probe the EEPROM; something fundamentally wrong on the I2C bus.

    read_eeprom() failure

    OMAP SD/MMC: 0

    reading u-boot.img

    reading u-boot.img

    U-Boot 2011.09 (Feb 09 2012 - 15:11:31)

    I2C:   ready

    DRAM:  256 MiB

    WARNING: Caches not enabled

    Could not probe the EEPROM; something fundamentally wrong on the I2C bus.

    NAND:  HW ECC Hamming Code selected

    256 MiB

    MMC:   OMAP SD/MMC: 0

    *** Warning - bad CRC, using default environment

    Net:   cpsw

    Hit any key to stop autoboot:  0

    SD/MMC found on device 0

    reading uEnv.txt

    ** Unable to read "uEnv.txt" from mmc 0:1 **

    reading uImage

    2922160 bytes read

    ## Booting kernel from Legacy Image at 80007fc0 ...

      Image Name:   Arago/3.1.0-psp04.06.00.03.sdk/a

      Image Type:   ARM Linux Kernel Image (uncompressed)

      Data Size:    2922096 Bytes = 2.8 MiB

      Load Address: 80008000

      Entry Point:  80008000

      Verifying Checksum ... OK

      XIP Kernel Image ... OK

    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.

    [    0.000000] Linux version 3.1.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Feb 9 14:58:49 CST 2012

    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f

    [    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

    [    0.000000] Machine: am335xevm

    [    0.000000] Memory policy: ECC disabled, Data cache writeback

    [    0.000000] AM335X ES1.0 (neon )

    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024

    [    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none

    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)

    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

    [    0.000000] Memory: 256MB = 256MB total

    [    0.000000] Memory: 253724k/253724k available, 8420k reserved, 0K highmem

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    [    0.000000]     DMA     : 0xffa00000 - 0xffe00000   (   4 MB)

    [    0.000000]     vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)

    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)

    [    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)

    [    0.000000]       .text : 0xc0008000 - 0xc0534000   (5296 kB)

    [    0.000000]       .init : 0xc0534000 - 0xc056d000   ( 228 kB)

    [    0.000000]       .data : 0xc056e000 - 0xc05c2d80   ( 340 kB)

    [    0.000000]        .bss : 0xc05c2da4 - 0xc05fd320   ( 234 kB)

    [    0.000000] NR_IRQS:396

    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts

    [    0.000000] Total of 128 interrupts on 1 active controller

    [    0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz

    [    0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz

    [    0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms

    [    0.000000] Console: colour dummy device 80x30

    [    0.000252] Calibrating delay loop... 498.89 BogoMIPS (lpj=2494464)

    [    0.058632] pid_max: default: 32768 minimum: 301

    [    0.058787] Security Framework initialized

    [    0.058911] Mount-cache hash table entries: 512

    [    0.059364] CPU: Testing write buffer coherency: ok

    [    0.064943] print_constraints: dummy:

    [    0.065416] NET: Registered protocol family 16

    [    0.065839] GPMC revision 6.0

    [    0.068434] OMAP GPIO hardware version 0.1

    [    0.071351] omap_l3_smx omap_l3_smx.0: couldn't find resource

    [    0.071983] omap_mux_init: Add partition: #1: core, flags: 0

    [    0.075915]  omap_i2c.1: alias fck already exists

    [    0.077914]  omap2_mcspi.1: alias fck already exists

    [    0.078202]  omap2_mcspi.2: alias fck already exists

    [    0.108230] bio: create slab <bio-0> at 0

    [    0.111092] SCSI subsystem initialized

    [    0.113178] usbcore: registered new interface driver usbfs

    [    0.113610] usbcore: registered new interface driver hub

    [    0.113876] usbcore: registered new device driver usb

    [    0.128784] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz

    [    0.131430] Advanced Linux Sound Architecture Driver Version 1.0.24.

    [    0.132799] Switching to clocksource gp timer

    [    0.138702] Switched to NOHz mode on CPU #0

    [    0.153967] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)

    [    0.154198] musb-hdrc musb-hdrc.0: dma type: pio

    [    0.155266] musb-hdrc musb-hdrc.0: USB OTG mode controller at d080a000 using PIO, IRQ 18

    [    0.155481] musb-hdrc musb-hdrc.1: dma type: pio

    [    0.156394] musb-hdrc musb-hdrc.1: USB OTG mode controller at d080c800 using PIO, IRQ 19

    [    0.156892] NET: Registered protocol family 2

    [    0.157131] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

    [    0.157488] TCP established hash table entries: 8192 (order: 4, 65536 bytes)

    [    0.157712] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

    [    0.157848] TCP: Hash tables configured (established 8192 bind 8192)

    [    0.157864] TCP reno registered

    [    0.157882] UDP hash table entries: 256 (order: 0, 4096 bytes)

    [    0.157914] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

    [    0.158159] NET: Registered protocol family 1

    [    0.158508] RPC: Registered named UNIX socket transport module.

    [    0.158527] RPC: Registered udp transport module.

    [    0.158540] RPC: Registered tcp transport module.

    [    0.158553] RPC: Registered tcp NFSv4.1 backchannel transport module.

    [    0.158828] NetWinder Floating Point Emulator V0.97 (double precision)

    [    0.172829] VFS: Disk quotas dquot_6.5.2

    [    0.172974] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

    [    0.173738] JFFS2 version 2.2. (NAND) (SUMMARY)  漏 2001-2006 Red Hat, Inc.

    [    0.174130] msgmni has been set to 495

    [    0.175096] io scheduler noop registered

    [    0.175115] io scheduler deadline registered

    [    0.175212] io scheduler cfq registered (default)

    [    0.176327] Could not set LED4 to fully on

    [    0.178344] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

    [    0.180531] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0

    [    0.659948] console [ttyO0] enabled

    [    0.664342] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1

    [    0.672205] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2

    [    0.680152] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3

    [    0.688026] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4

    [    0.695892] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5

    [    0.715574] brd: module loaded

    [    0.725348] loop: module loaded

    [    0.728881] i2c-core: driver [tsl2550] using legacy suspend method

    [    0.735432] i2c-core: driver [tsl2550] using legacy resume method

    [    0.741921] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write

    [    0.802852] No daughter card found

    [    0.806486] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write

    [    0.872853] AM335X: EVM Config read fail: -110

    [    0.879593] mtdoops: mtd device (mtddev=name/number) must be supplied

    [    0.886727] omap2-nand driver initializing

    [    0.891289] OneNAND driver initializing

    [    0.897234] CAN device driver interface

    [    0.901246] CAN bus driver for Bosch D_CAN controller 1.0

    [    0.907891] usbcore: registered new interface driver cdc_ether

    [    0.914313] usbcore: registered new interface driver cdc_subset

    [    0.920593] Initializing USB Mass Storage driver...

    [    0.925999] usbcore: registered new interface driver usb-storage

    [    0.932316] USB Mass Storage support registered.

    [    0.937259] musb-hdrc musb-hdrc.1: MUSB HDRC host driver

    [    0.942944] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1

    [    0.950863] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

    [    0.958033] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    [    0.965645] usb usb1: Product: MUSB HDRC host driver

    [    0.970865] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd

    [    0.976461] usb usb1: SerialNumber: musb-hdrc.1

    [    0.982217] hub 1-0:1.0: USB hub found

    [    0.986231] hub 1-0:1.0: 1 port detected

    [    0.991672] mousedev: PS/2 mouse device common for all mice

    [    0.998981] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0

    [    1.006021] i2c /dev entries driver

    [    1.012538] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec

    [    1.019577] cpuidle: using governor ladder

    [    1.024586] cpuidle: using governor menu

    [    1.032424] usbcore: registered new interface driver usbhid

    [    1.038347] usbhid: USB HID core driver

    [    1.043631] usbcore: registered new interface driver snd-usb-audio

    [    1.052162] ALSA device list:

    [    1.055352]   No soundcards found.

    [    1.058926] oprofile: hardware counters not available

    [    1.064248] oprofile: using timer interrupt.

    [    1.068767] nf_conntrack version 0.5.0 (3964 buckets, 15856 max)

    [    1.075696] ip_tables: (C) 2000-2006 Netfilter Core Team

    [    1.081426] TCP cubic registered

    [    1.084872] NET: Registered protocol family 17

    [    1.089558] can: controller area network core (rev 20090105 abi 8)

    [    1.096188] NET: Registered protocol family 29

    [    1.100864] can: raw protocol (rev 20090105)

    [    1.105372] can: broadcast manager protocol (rev 20090105 t)

    [    1.111369] Registering the dns_resolver key type

    [    1.116414] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3

    [    1.124499] ThumbEE CPU extension supported.

    [    1.129898] _regulator_get: mpu.0 supply mpu not found, using dummy regulator

    [    1.137559] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=500000000 v=1100000)on vddmpu

    [    1.146822] omap2_set_init_voltage: unable to set vdd_mpu

    [    1.155345] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)

    [    1.164733] Waiting for root device /dev/mmcblk0p2...

  • AM335x的evm板不要拆开使用,因为有些电源是依赖daughter board的

  • Hi,alvin

    driver下面应该是添加了nandflash的驱动,你检查看看你的board-am335xevm.c文件中是否初始化了nandflash,并且执行了。

    Thanks

    Best Regards

    John

  • 这是读不到IIC的EEPROM的值导致的。TI的文档还是需要细细的读啊。

  • 我今天也遇到类似问题,电路和TI的EVM板一样,电源都正常,用TI的sd 卡Uboot, 结果跑不起来,串口打印是乱码。测试TI EVM的BASEBOARD,不连接GP板和LCD, 结果一样也无法从SD卡Uboot, 串口打印没有任何信息,还不知道是什么原因,急待TI 高手指点。

  • baseboard的确是不能单独启动,我记得是因为串口的一个片子的供电在daughterboard上,这点。。。 我也觉得不爽。你的板子,如果不能启动,您先查查boot config

  • 请问兄台这个问题解决了吗?

    我的问题与你如出一辙~~

  • 你在本论坛中搜索下,有一篇文章专门介绍如何在nand中烧写ubifs文件

  • TI的BSP貌似是直接可以的,在board-am335xevm.c中加入nandflash和管脚的初始化应该是可以的。

    我们自己做的板子用的UBIFS跑得很好