之前dm368的DDR和Flash的选型分别是MT47H64M16HR-3-IT K9F2G08U0B,现在想更换DDR和Flash的型号分别为EM68C16CWQG-25IH W29N02GVSI,硬件上是pin2pin的,想咨询下368是否支持这样的型号?软件上要怎样去修改?之前有看到368 flash选型有关于nand flash id的设置,flash的选型时一定要在他给的id list里面去选吗?谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前dm368的DDR和Flash的选型分别是MT47H64M16HR-3-IT K9F2G08U0B,现在想更换DDR和Flash的型号分别为EM68C16CWQG-25IH W29N02GVSI,硬件上是pin2pin的,想咨询下368是否支持这样的型号?软件上要怎样去修改?之前有看到368 flash选型有关于nand flash id的设置,flash的选型时一定要在他给的id list里面去选吗?谢谢!!!
你好,
对于DDR,你可以在DM368的数据手册里面找到下面的内容,所以符合JESD79D-2A的DDR2,DM36x都是可以支持的。
It supports JESD79D-2A standard compliant DDR2 SDRAM devices and compliant Mobile DDR SDRAM devices.
对于nand,如果你需要支持nand启动,请参考arm subsystem guide里面的关于启动的相关章节里面的nand list,选择在这个列表里面的nand。