你好:
我使用的开发板是AM437X IDK。在CCS条件下进行编程。我直接将C:\ti\pdk_am437x_1_0_5\packages\ti\starterware\binary\dmtimer_app_cdt\bin\am43xx-evm\gcc。目录下的已经编译完成的文件通过SD卡下载进入开发板中,程序可以正常进入中断计数。
但是我把该工程移植到TIDEP0057中提供的程序工程文件中,移植以后程序可以编译成功,但是下载进去以后,程序进不了中断。不清楚这是为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
我使用的开发板是AM437X IDK。在CCS条件下进行编程。我直接将C:\ti\pdk_am437x_1_0_5\packages\ti\starterware\binary\dmtimer_app_cdt\bin\am43xx-evm\gcc。目录下的已经编译完成的文件通过SD卡下载进入开发板中,程序可以正常进入中断计数。
但是我把该工程移植到TIDEP0057中提供的程序工程文件中,移植以后程序可以编译成功,但是下载进去以后,程序进不了中断。不清楚这是为什么?
但是我使用C:\ti\pdk_am437x_1_0_5\packages\ti\starterware\binary\dmtimer_app_cdt\bin\am43xx-evm\gcc。他提前编译好的二进制文件通过SD卡下载进开发板可以使用啊。所以代码应该不会出问题把,编译的代码应该就是这一份啊。我移植过去以后也没有落下什么东西,我仔细看了,该配置的都配置了。但是进不去中断,是因为我移植的工程里面跑了操作系统,建立了系统任务有关吗?该工程是TIDEP0057下面提供的 Tidcbv9 project 。
你好:
/* Perform initialization of Interrupt controller*/
status = INTCInit(FALSE);
int32_t DMTimerAppIntrConfig(dmtimerAppCfg_t *pDmtimerObj)
{
/* Precondition : Enable ARM interrupt control and initialise the Interrupt
Controller. */
/* local Structure which holds the Interrupt parameters. */
intcIntrParams_t intrParams;
int32_t returnVal = S_PASS;
intrParams.triggerType = pDmtimerObj->trigType;
/* Currently hard coded priority number */
intrParams.priority = 0x20U;
intrParams.pFnIntrHandler = pDmtimerObj->pFnIntrHandler;
/* Pointer to the app object being passed to handler */
intrParams.pUserParam = pDmtimerObj->pUserParam;
/* Currently hard coded - non secure mode */
intrParams.isIntrSecure = FALSE;
returnVal = INTCConfigIntr(pDmtimerObj->intrLine, &intrParams,FALSE);
return (returnVal);
}
if (NULL!= pDmtimerObj->pFnIntrHandler)
/*there is an Interrupt handler to be installed */
{
/* Enable the DMTimer interrupts */
DMTimerIntEnable(pDmtimerObj->instAddr, pDmtimerObj->intrMask);
}
中断配置信息都有了,中断也已经使能了啊。但是还是进不去。