This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 采集模式提问



请问可以解释一下 这些采集模式的具体解释吗? typedef enum { SYSTEM_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_EMBEDDED_SYNC = 0, /**< Single Channel non multiplexed mode */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_MULTI_CH_LINE_MUX_EMBEDDED_SYNC, /**< Multi-channel line-multiplexed mode */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_MULTI_CH_PIXEL_MUX_EMBEDDED_SYNC, /**< Multi-channel pixel muxed */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_HSYNC_VBLK, /**< Single Channel non multiplexed discrete sync mode with HSYNC and VBLK as control signals. */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_HSYNC_VSYNC, /**< Single Channel non multiplexed discrete sync mode with HSYNC and VSYNC as control signals. */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_ACTVID_VBLK, /**< Single Channel non multiplexed discrete sync mode with ACTVID and VBLK as control signals. */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_ACTVID_VSYNC, /**< Single Channel non multiplexed discrete sync mode with ACTVID and VBLK as control signals. */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_MULTI_CH_LINE_MUX_SPLIT_LINE_EMBEDDED_SYNC, /**< Multi-channel line-multiplexed mode - split line mode */ SYSTEM_CAPT_VIDEO_CAPTURE_MODE_MAX /**< Maximum modes */ } System_CaptVideoCaptureMode;

  • 多达3个可编程高清视频图像协处理器(HDVICP2)引擎

    • 编码、解码、码转换操作
    • H.264,MPEG2,VC1,MPEG4 SP/ASP
    高清视频处理子系统(HDVPSS)
    • 2个165MHz HD视频捕捉通道
      • 1个16/24bit和1个16bit通道
      • 每个通道可被分成双8bit捕捉通道
    • 2个165MHz HD视频显示通道
      • 1个16/24/30bit和1个16bit通道
    • 同时存在的SD和HD模拟输出
    • 高达165MHz像素时钟的带HDCP的HDMI1.3发送器
    • 具有扫描方式/格式/速率转换等高级视频处理功能
    • 三个图层和符合器

  • 请问一下 8168接TVP5185,我想一个8bit通道分时复用两路视频,应该选择哪种模式呢?

  • 还有请问一下 这种模式

    SYSTEM_CAPT_VIDEO_CAPTURE_MODE_MULTI_CH_PIXEL_MUX_EMBEDDED_SYNC

    一个8bit的通道,可以传几路视频?