This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368



你好,我现在把cmem.c放到内核中,且我的DDR是256M,所以我在bootargs中将mem = 128M,在cmem,c中修改如下

/* Register the module parameters. */
MODULE_PARM_DESC(phys_start, "\n\t\t Start Address for CMEM Pool Memory");
static char *phys_start = "0x88000000"; //128M ARM
MODULE_PARM_DESC(phys_end, "\n\t\t End Address for CMEM Pool Memory");
static char *phys_end = "0x8FFFFFFF"; //128M DSP
module_param(phys_start, charp, S_IRUGO);
module_param(phys_end, charp, S_IRUGO);

static int npools[NBLOCKS] = {0, 0};

static char *pools[MAX_POOLS] = {
NULL
};

现在执行正常,

请问这样修改可以吧,还有我想配置一些内存池,应该配成多大多少个,哪里有参考,还有

MODULE_PARM_DESC(phys_start_1, "\n\t\t Start Address for Extended CMEM Pool Memory");
static char *phys_start_1 = NULL;
MODULE_PARM_DESC(phys_end_1, "\n\t\t End Address for Extended CMEM Pool Memory");
static char *phys_end_1 = NULL;
module_param(phys_start_1, charp, S_IRUGO);
module_param(phys_end_1, charp, S_IRUGO);

static char *pools_1[MAX_POOLS] = {
NULL,
};

请问这块代码是干什么用的,是扩展内存用的吗?

谢谢!!!