This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF通信的时序问题



在EMIF通信过程中,两个片选信号对应一个地址信号,请问这有可能会是什么问题呢???求解答,谢谢!

  • EMIF的片选信号会映射到不同的地址空间,可以看一下数据手册里的memory map。每次EMIF读写操作,只会选通一个片选信号,不会出现两个片选信号同时选通的情况。

  • 恩恩,之前时序好像出了问题,但是现在相邻地址的增量是8,下图所示:

    请问这是怎么回事儿呢??


      

  • 请问代码怎么写的?

  • /************************异步等待配置**************/
    	/* Assign values to async wait config structure */
    	//asyncWaitConfig.waitPol    = CSL_EMIF_WP_LOW;//与NAND有关,不用设置
    	asyncWaitConfig.waitPin    = waitPin;
    	asyncWaitConfig.waitCycles = CSL_EMIF_ASYNCWAITCFG_WAITCYCLE_DEFAULT;//默认值为0x80
    
    /***************对异步传输的初始化配置的过程************/
    	/* Assign values to nand async config structure */
    	asyncConfig.selectStrobe = CSL_EMIF_ASYNCCFG_SELECTSTROBE_DEFAULT;
    	asyncConfig.ewMode       = CSL_EMIF_ASYNCCFG_WEMODE_DEFAULT;
    	asyncConfig.w_setup      = CSL_EMIF_ASYNCCFG_WSETUP_DEFAULT;
    	asyncConfig.w_strobe     = CSL_EMIF_ASYNCCFG_WSTROBE_DEFAULT;
    	asyncConfig.w_hold       = CSL_EMIF_ASYNCCFG_WHOLD_DEFAULT;
    	asyncConfig.r_setup      = CSL_EMIF_ASYNCCFG_RSETUP_DEFAULT;
    	asyncConfig.r_strobe     = CSL_EMIF_ASYNCCFG_RSTROBE_DEFAULT;
    	asyncConfig.r_hold       = CSL_EMIF_ASYNCCFG_RHOLD_DEFAULT;
    	asyncConfig.turnAround   = CSL_EMIF_ASYNCCFG_TAROUND_DEFAULT;
    	asyncConfig.aSize        = CSL_EMIF_ASYNCCFG_ASIZE_DEFAULT;
    
    
    /*****************对异步传输进行emif配置************/
    	/* Assign values to config structure */
    	asyncCfg.chipSelect   = chipSel;
    	//应该是需要加RAMwidth的,而且还有emifopmode工作模式,在CSL_NandConfig里面有定义这两部分,看看其他结构体里面有没有
    	//nandCfg.nandWidth     = CSL_EMIF_8_BIT;//还需不需要定义RAM的width
    	//nandCfg.nandPageSize  = CSL_NAND_PAGESZ_512;//这个应该不用了吧,没有page
    	asyncCfg.emifAccess   = CSL_EMIF_16BIT;//改成了16位
    	nandCfg.emifOpMode    = CSL_EMIF_OPMODE_POLLED;
    	//nandCfg.nandType      = CSL_NAND_SMALL_BLOCK;//同样不需要
    	asyncCfg.asyncWaitCfg = &asyncWaitConfig;
    	asyncCfg.asyncCfg     = &asyncConfig;
    
    /********************进行配置*********************/
    	/* Configure Asynchronous settings */
    	status = EMIF_asyncConfig(hEmif, &asyncCfg);        //在这里面需要把RAMwidth和EMIFopmode加进去
    		if(status != CSL_SOK)
    		{
    			printf("EMIF Asynchronous Config Failed!!\n");
    			return(result);
    		}


    这是EMIF配置部分,是通过例程修改的,现在地址增量是1,但是每此数据都是读两遍,不知道是怎么回事。

  • 请看一下ESCR寄存器的BYTEMODE是否设成了0?

  • 恩恩,bytemode是设置成00了的

  • 看一下时序图是否跟你配置的一致?