This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6747的EMIFA访问外部16位异步存储设备的地址总线问题



大家好,我要使用C6747的EMIFA访问外部16位异步存储设备,现在要让片选cs4有效,EMA_A12位为1,根据手册上的图

16位模式下,EMA_A12位对应的是外部设备地址的A13位,片选cs4有效起始地址为0x6400 0000,那么要让EMA_A12为1,地址的第13位(从0开始数)应该是1才对,也就是访问的地址要为0x6400 2000,这时A13为1,但为什么我测试的时候,访问0x6400 2000时EMA_A12信号线还是为0,而访问0x6400 4000时EMA_A12才能为1,是我理解错了吗