This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 SRIO NREAD中断配置问题



现在使用的是官方提供的:K1_STK_v1.1下SRIO驱动,用于测试SRIO通信。
对原代码SRIO_Loopback_Mode loopback_mode= SRIO_NO_LOOPBACK;流程进行修改,实现了c6678与FPGA之间的数据通信(数据通信功能已测试完成)。

现在的问题是,原代码中可以正常接收到doorbell中断(即FPGA向C6778发送doorbell,在c6678一侧会成功引起中断),整理了相关函数主要有以下几个:
SRIO_Interrupts_Init();
KeyStone_SRIO_Interrupt_init(srio_cfg->interrupt_cfg);
interrupt void SRIO_Doorbell_ISR() // 中断执行函数

在原测试实例流程中,我们进行了NREAD操作,完成KeyStone_SRIO_LSU_transfer(&lsuTransfer);配置后通过KeyStone_SRIO_wait_LSU_completion轮询等待
读操作是否完成。
现在我们想修改为中断触发形式来给出传输完成提示,对应的中断想使用“LSU0_Transaction_Complete_OK”

请问各位专家应该具体修改代码哪些地方可实现上述功能?