This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138串口烧写UBL、UBOOT问题

Other Parts Discussed in Thread: OMAP-L138, AM1808

问题:

我使用sfh_OMAP-L138.exe串口烧写工具来烧写UBL、UBOOT时,在擦除的过程中总是停止在Waiting for SFT on the OMAP-L138...这,具体信息如下:

C:\temp>sfh_OMAP-L138 -erase -targetType AM1808 -flashType SPI_MEM -v -p Com8

-----------------------------------------------------

  TI Serial Flasher Host Program for OMAP-L138

  (C) 2012, Texas Instruments, Inc.

  Ver. 1.67

-----------------------------------------------------

     [TYPE] Global erase

   [TARGET] AM1808

   [DEVICE] SPI_MEM

[SPI Block] 0

Attempting to connect to device Com7...

Press any key to end this program at any time.

(AIS Parse): Read magic word 0x41504954.

(AIS Parse): Waiting for BOOTME... (power on or reset target now)

(AIS Parse): BOOTME received!

(AIS Parse): Performing Start-Word Sync...

(AIS Parse): Performing Ping Opcode Sync...

(AIS Parse): Processing command 0: 0x58535901.

(AIS Parse): Performing Opcode Sync...

(AIS Parse): Loading section...

(AIS Parse): Loaded 8552-Byte section to address 0x80000000.

(AIS Parse): Processing command 1: 0x58535901.

(AIS Parse): Performing Opcode Sync...

(AIS Parse): Loading section...

(AIS Parse): Loaded 116-Byte section to address 0x80002168.

(AIS Parse): Processing command 2: 0x58535901.

(AIS Parse): Performing Opcode Sync...

(AIS Parse): Loading section...

(AIS Parse): Loaded 768-Byte section to address 0x800021DC.

(AIS Parse): Processing command 3: 0x58535906.

(AIS Parse): Performing Opcode Sync...

(AIS Parse): Performing jump and close...

(AIS Parse): AIS complete. Jump to address 0x80000000.

(AIS Parse): Waiting for DONE...

(AIS Parse): Boot completed successfully.

Waiting for SFT on the OMAP-L138...

说明:

uboot 和linux的默认调试口为 UART2 ,之前我用 UART2作为调试口的时候一切都很顺利,现在因为硬件的影响 想用 UART0 作为调试口,就出现了上述的问题 Waiting for SFT on the OMAP-L138...

希望可以给点思路

TKS