方法1:参考这篇文章 www.deyisupport.com/.../365348.aspx
在执行步骤2时(devmem2 0x48044038 w 0x1842),出错,如下
/dev/mem opened.[ 3175.118330] Unhandled fault: external abort on non-linefetch (0x1018) at 0xb6f3e038 [ 3175.127296] ------------[ cut here ]------------ [ 3175.131948] WARNING: CPU: 0 PID: 1697 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x234/0x35c() [ 3175.141555] 44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET L4_PER_0 (Read): Data Access in User mode during Functional access [ 3175.153688] Modules linked in: btwilink bluetooth ads7846 c_can_platform c_can dwc3_omap can_dev snd_soc_davinci_mcasp 6lowpan_iphc [last unloaded: dmtimer_pwm] [ 3175.168167] CPU: 0 PID: 1697 Comm: devmem2 Tainted: G O 3.14.43 #6 [ 3175.175243] Backtrace: [ 3175.177720] [<c001115c>] (dump_backtrace) from [<c00112f8>] (show_stack+0x18/0x1c) [ 3175.185318] r6:00000093 r5:00000009 r4:ddf65db0 r3:00000000 [ 3175.191038] [<c00112e0>] (show_stack) from [<c06144f0>] (dump_stack+0x20/0x28) [ 3175.198298] [<c06144d0>] (dump_stack) from [<c00375f4>] (warn_slowpath_common+0x6c/0x8c) [ 3175.206424] [<c0037588>] (warn_slowpath_common) from [<c00376b8>] (warn_slowpath_fmt+0x38/0x40) [ 3175.215155] r8:c06422a0 r7:c07b1df8 r6:c07b1a04 r5:80080003 r4:ddcd9f90 [ 3175.221918] [<c0037684>] (warn_slowpath_fmt) from [<c02823ac>] (l3_interrupt_handler+0x234/0x35c) [ 3175.230824] r3:ddccd300 r2:c07b1ac4 [ 3175.234433] [<c0282178>] (l3_interrupt_handler) from [<c0063ce0>] (handle_irq_event_percpu+0x54/0x1bc)
Q1:这个怎么解决
方法2:在free-electrons有关于timer的代码 http://lxr.free-electrons.com/source/drivers/pwm/pwm-omap-dmtimer.c?v=4.5
编译通过后,但加载驱动时报错,如下
[ 361.851324] omap-dmtimer-pwm dmtimer-pwm@4: Missing dmtimer platform data
[ 361.858169] omap-dmtimer-pwm: probe of dmtimer-pwm@4 failed with error -22
Q2:这个是设备树的问题吗?
Q3:有没有关于TIMER产生PWM的demo啊