This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Chain堵塞造成帧数下降



目前正在进行DSP的图像算法开发

在DSP的部分接了3个link

Camera->MCTNF->VNF->A_DSPLink->B_DSPLink->C_DSPLink->DUP->sclr->…

其中,当enable C_DSPLink的功能时所要耗费的时间比较长,大约是16~18ms

Disable C_DSPLink时仅传递frame,并没有进行计算,耗费时间在2ms以下

发现在多次enable和Disable切换时,会导致camera link端得帧数下降

原先disable时可以达到约47fps,下降至30fps

原先enable时可以达到约42fps,下降至20fps

且帧数固定,感觉像是有frame卡住了没有归还给camera link

可是一直找不到根本原因,

已经尝试将每个link中的frame buffer加大:

SYSTEM_LINK_FRAMES_PER_CH    (8)

但仍然没效果

 

请教各为前辈!!