This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急求帮助!DSP6655的GPIO17中断无法响应



DSP6655的GPIO17引脚设为普通IO下降沿触发,对应CIC中断控制器输入事件号1,映射到channel 1和out1。

当手动触发给偏移0x20寄存器赋值0x01时,0x200寄存器status相应位置位并且进入中断服务函数。而当外部GPIO17产生下降沿时(用示波器看确定产生了),没有响应。

同时映射了事件145   TINT4L到CIC_OUT2可以正常进入中断服务函数。

关于GPIO的配置,对GPIO15用相同的配置函数可以产生中断并进入相应的服务函数,区别只是一个直接进入核中断控制器一个经过CIC产生事件再进入中断控制器。

请问,1.GPIO16-31的外部信号可以产生中断信号吗?GPIO文档中寄存器高16位保留。

2.外部产生的信号和DSP内部产生的信号在映射CIC时有什么区别吗?

谢谢各位大神