求教!
在DSPLIB中,给出了FFT的示例工程,有这样几个工程。请问其中,DSPF_dp_fftDP*DP_66_LE_COFF和DSPF_sp_fftSP*SP_66_LE_COFF,以及DSPF_sp_fftSP*SP_66_LE_ELF之间的区别是什么呢?另外,这些例程中的FFT程序是一维的,是支持任意长度一维数组的FFT吗?还是只能是2的幂大小的一维的FFT?
谢谢指导!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求教!
在DSPLIB中,给出了FFT的示例工程,有这样几个工程。请问其中,DSPF_dp_fftDP*DP_66_LE_COFF和DSPF_sp_fftSP*SP_66_LE_COFF,以及DSPF_sp_fftSP*SP_66_LE_ELF之间的区别是什么呢?另外,这些例程中的FFT程序是一维的,是支持任意长度一维数组的FFT吗?还是只能是2的幂大小的一维的FFT?
谢谢指导!
DSPF_dp_fftDP*DP_66_LE_COFF是double point, little endian, COFF格式。
DSPF_sp_fftSP*SP_66_LE_COFF是single point, little endian, COFF格式。
DSPF_sp_fftSP*SP_66_LE_ELF是single point, little endian, ELF格式。
支持2的幂大小的一维fft,2d, 3d fft可以下载下面的FFTlib。
http://www.ti.com/tool/FFTLIB