您好:
1. 8核跑一个APP,在debug的时候,是否需要8个核都加在一个gel文件去初始化DDR,我的代码是放在DDR里面的?
2. 如何去看每个核创建的线程,为什么我试图打开ROV,一直显示一个进度条,打不开,而且这样CCS极易死机?
3. 我使用的是6678LE的开发板,我看上面是4块DDR,但是为什么我设置成o=0x80000000,len=0x80000000,这样debug会出错,只使用512M的DDR没有问题
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
1. 8核跑一个APP,在debug的时候,是否需要8个核都加在一个gel文件去初始化DDR,我的代码是放在DDR里面的?
2. 如何去看每个核创建的线程,为什么我试图打开ROV,一直显示一个进度条,打不开,而且这样CCS极易死机?
3. 我使用的是6678LE的开发板,我看上面是4块DDR,但是为什么我设置成o=0x80000000,len=0x80000000,这样debug会出错,只使用512M的DDR没有问题
谢谢!
1. core0去初始化一次就可以了。
2. 是否按照下面的链接使用ROV?
http://rtsc.eclipse.org/docs-tip/RTSC_Object_Viewer
3. 6678LE开发板上总共是512M DDR3。
http://www2.advantech.com/Support/TI-EVM/6678le_of.aspx