This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455的EMIF传输问题



背景介绍:
芯片:DSP:C6455,FPGA:XCV5
每帧数据量:320*300*16bit
传输方式:EMIF 32位传输 异步传输 外部空间CE2
DSP内部时钟:1GHz
数据频率:50Hz

1、由于每一帧的数据量有些大,FPGA存储空间限制,无法一次性写入CE2,分300次写入,每次写入160*32bit,
利用for循环300次,使用mymcpy读取,读取完一帧数据需要3.6*10^6个时钟周期,优化后需要1.7*10^6个时钟
周期,超时严重,无法满足实时性要求;
2、在使用优化后,传输时,每一个32位数据会被读取两次,即在一个CE下拉周期中,AOE下拉两次;

请问:1、有没有其他方式实现EMIF读取,比如DMA读取方式,速度会不会变快
2、如何解决优化时,在一个CE下拉周期中,AOE下拉两次的问题