最近在使用AM1808做一个项目,打算使用GPIO模拟一个CLK信号输出,不知道AM1808的GPIO翻转速度最大是多少?能否模拟输出一个8MHz的CLK信号输出?希望有了解这一块的大神指点一二,感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
够呛
而且没有实时性,你CPU如果跑别的任务,这速度会有很大变化
建议用PWM模块来做
PWM参数
| PARAMETER | TEST CONDITIONS | 1.3V, 1.2V | 1.1V | 1.0V | UNIT | ||||
|---|---|---|---|---|---|---|---|---|---|
| MIN | MAX | MIN | MAX | MIN | MAX | ||||
| tw(PWM) | Pulse duration, PWMx output high/low |
20 | 20 | 26.6 | ns | ||||
| tw(SYNCOUT) | Sync output pulse width |
8tc(SCO) | 8tc(SCO) | 8tc(SCO) | cycles | ||||
| td(PWM)TZA | Delay time, trip input active to PWM forced high Delay time, trip input active to PWM forced low |
no pin load; no additional programmable delay | 25 | 25 | 25 | ns | |||
| td(TZ-PWM)HZ | Delay time, trip input active to PWM Hi-Z |
no additional programmable delay | 20 | 20 | 20 | ns | |||
或者timer
| NO. | 1.3V, 1.2V, 1.1V, 1.0V | UNIT | |||
|---|---|---|---|---|---|
| MIN | MAX | ||||
| 1 | tc(TM64Px_IN12) | Cycle time, TM64Px_IN12 | 4P | ns | |
| 2 | tw(TINPH) | Pulse duration, TM64Px_IN12 high | 0.45C | 0.55C | ns |
| 3 | tw(TINPL) | Pulse duration, TM64Px_IN12 low | 0.45C | 0.55C | ns |
| 4 | tt(TM64Px_IN12) | Transition time, TM64Px_IN12 | 0.05C or 10(3) | ns | |