你好,我最近在调试dm8168板子用的开发包是DVRRDK_02.00.00.23,采用十六路模拟入,HDMI1080P@60出,其中输入用的是tvp5158 芯片,四路模拟入输出一路8位数字输出10M,我发现我用720X576摄像头视频正常,但是我当前项目要求用960X576的模拟入摄像头,视频正常,但是视频出现上下抖动状况,请问是什么原因,是tvp5158不支持这种格式输入吗?
谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我最近在调试dm8168板子用的开发包是DVRRDK_02.00.00.23,采用十六路模拟入,HDMI1080P@60出,其中输入用的是tvp5158 芯片,四路模拟入输出一路8位数字输出10M,我发现我用720X576摄像头视频正常,但是我当前项目要求用960X576的模拟入摄像头,视频正常,但是视频出现上下抖动状况,请问是什么原因,是tvp5158不支持这种格式输入吗?
谢谢!!!
你好:
如果我不用TVP5158,改用其他支持WD1(960H)芯片去实现四路视频分时复用一个输入,我看手册有这句话
“Two independent video capture input ports up to 165 MHz, each VIP instance supports scaling, pixel format conversion, and up to one 1080P60 or 8-channel multiplexed D1 data.” 4路D1是108M ,4路WD1是144M,小于165M。
请问,dm8168能支持16路WD1标清输入吗,在哪里修改输入分辨率配置。还是dm8168自动识别WD1分辨率?
谢谢!!!
你好,
请参考dvr rdk 4.01里面的multich_hybrid_dvr.c,有对960H的支持。
http://www.radiumboards.com/dvr-DM8168-960H-ds-v0.3.pdf