This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关C66XX编译问题



编译出来提示不能加载和运行到目标系统,有以下二个问题:

1、tdata段添加到cmd文件也一样提示

Description Resource Path Location Type
#10247-D creating output section ".tdata" without a SECTIONS specification IntelligenceBox C/C++ Problem

2、__c6xabi_errno_addr重定位问题

Description Resource Path Location Type
<a href="processors.wiki.ti.com/.../17003"> errno.c relocation from function "__c6xabi_errno_addr" to symbol "__errno" overflowed; the 32-bit relocated address 0x8001b5bc is too large to encode in the 15-bit unsigned field (type = 'R_C6000_TPR_U15_B' (38), file = "C:\ti\ccsv6\tools\compiler\ti-cgt-c6000_8.1.1\lib\rts6600_elf_mt.lib<errno.obj>", offset = 0x0000000c, section = ".text:__c6xabi_errno_addr") IntelligenceBox line 87 C/C++ Problem

请问以上两个问题怎么解决?