在/sys/class/gpio/下操作export,以及对应gpion文件夹下的direction
譬如,当echo “out” > direction时,引脚自动变成低电平了,是否可以修改这个默认状态?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在/sys/class/gpio/下操作export,以及对应gpion文件夹下的direction
譬如,当echo “out” > direction时,引脚自动变成低电平了,是否可以修改这个默认状态?
不建议这样改动,会带来一定危险性,
如果你要特定某一个引脚默认输出高电平,可以在内核引导的时候,配置该引脚输出高电平,在devicetree文件修改,如gpio0_7,增加:
&gpio0 {
/* Do not idle the GPIO used for holding the VTT regulator */
ti,no-reset-on-init;
ti,no-idle-on-init;
p7 {
gpio-hog;
gpios = <7 GPIO_ACTIVE_HIGH>;
output-high;
line-name = "FET_SWITCH_CTRL";
};
};
你好,这样的话,sys/class/gpio就不能再导出对应的gpio了,也就是不能通过echo "out" > direction和echo 0 > value或者echo 1 > value来控制了。我其实目的是,当我执行“echo "out" > direction”时,gpio0_2引脚不要自作聪明地帮我输出低电平,而是要输出高电平或者保持原本电平。