This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti-processor-sdk-linux安装完成setup.sh时 报uboot-mkimage 没有可安装候选。



RT。

=============================================以下是输出======================================================

Performing sudo apt-get install xinetd tftpd nfs-kernel-server minicom build-essential libncurses5-dev dos2unix screen lrzsz uboot-mkimage
正在读取软件包列表... 完成
正在分析软件包的依赖关系树
正在读取状态信息... 完成
没有可用的软件包 uboot-mkimage,但是它被其它的软件包引用了。
这可能意味着这个缺失的软件包可能已被废弃,
或者只能在其他发布源中找到
然而下列软件包会取代它:
u-boot-tools:i386 u-boot-tools

E: 软件包 uboot-mkimage 没有可安装候选
Failed setup, aborting..
Failed setup, aborting..

=============================================以上是输出======================================================

请问需要单独apt  u-boot-tools:i386么?或者需要把安装目录/home/ti-processor-sdk-linux/bin 加入路径?

谢谢。

PS:安装环境是 真机 Ubuntu16.04 和 VMware Workstation 10下安装的Xubuntu16.04。均出现同一问题。

PS2:“If using a virtual machine as your Linux host, you will likely need to import the target board into the virtual machine as a mass storage device.”

拿目标板做 mass storage device?这是什么意思?,mass storage device不是U盘一类么?