This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用OMAPL138EZWT的LCD模块显示界面时会发生界面整体漂移

Other Parts Discussed in Thread: AM1808

1. 使用是的OMAPL138EZWT 62A69EW芯片

2. 原理图是采用的参考设计

3. 采用的什么SDK我现在没办法得知,运行的是VxWorks5.5.1的操作系统

4. 电脑操作系统的WIN7

5. 开发的编译器是使用的Tornado2.2,

6. 开发已经结束,在开发也遇到了问题的,但认为应该可以解决所以放到现在来解决

7. 对这款芯片有一些了解,但不多。

8. 问题描述:我们的电路板有网络通信和LCD显示的功能,电路板正常运行时,LCD屏幕上的显示一切正常,这两个功能单独使用是都没有问题的,但是网络连接上的时候,比如使用FTP客户端连接到VxWorks操作系统时,LCD显示屏的界面就会发生整体漂移的现象,这时查看LCD的显存数据,都是正确的,这时如果对RASTER_CTRL寄存器的RASTER_EN = 0(Disable the LCD Raster controller),延时32毫秒,再把RASTER_EN = 1(Enable the LCD RAster controller),这时LCD显示板就会恢复。软件上看,网络连接上与LCD的显示上没有什么关联,不太像代码编程错误造成的LCD显示的问题,感觉像是什么操作影响了LCD模块的正常工作。应该也不是LCD显示屏本身在的问题,我换过三种屏测试,都存在同样的问题。基于AM1808的控制板也遇到过同样的问题,不运行操作系统时,裸跑时,有同事说以前测试时也会产生。