This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5158后级无法识别

Other Parts Discussed in Thread: TVP5158

我正在使用TI的TVP5158,在调试中有

如下问题:设置为CH1单路A/D,VO_A输出8BIT的D1信号,

但后级无法识别,请问是什么原因以及我后续该如何做?谢谢!

  • 你好,

    你是否有测量过TVP5158输出的时钟正确,数据线上有数据输出?

  • 你好!附件是TVP5158的寄存器设置,工作模式

    是模拟CVBS输入通道1,输入PAL信号,输出选择DVO_1,

    格式为8BIT DI格式,但后级的并串转换芯片不识别。

    将标准DI信号接到并串芯片输入端口,是可以正常工作

    的。

    寄存器设置:
    信号链路:

    CVBS IN ----- TVP5158 -----FPGA -----GS2972


    1.当前状态:
    将TVP5158设置成单路模式,输出的信号经GS2972后无法检测到。
    TVP5158输出时钟:27M;
    TVP5158的DVD_A口输出数据进入FPGA后提取的HS,VS,OE正常;
    但去掉输入CVBS后,HS,VS,OE扔正常存在;

    其它测试:FPGA用TVP5158输出的27M时钟生成彩条测试图,可正常被GS2972检测到;
    且正常显示输出。


    2.TVP5158设置内容:
    在DVD_A口输出TVP5158自身生成的蓝场测试信号。
    格式:8BITS的D1格式。PAL制。

    TVP5158寄存器如下:
    00H: 7e b0 03 00 02 00 00 00 51 58 71 02 82 00 ff 03
    10H: 80 80 00 80 00 00 70 0a 40 00 00 00 0c 00 00 00
    20H: 6a 08 80 80 00 f5 00 00 00 06 1e 04 00 f2 08 04
    30H: ff ff 00 00 6a 08 05 07 84 00 d0 02 19 00 20 01
    40H: 07 00 47 00 04 00 07 00 84 00 d0 02 6f 02 18 00
    50H: 84 00 d0 02 97 00 bc 02 26 00 06 01 1e 09 34 03
    60H: 00 09 40 1e 18 00 0b 00 00 1f 1f 02 10 04 64 20
    70H: 7d 00 8a 64 04 02 0f 0f 03 05 20 1e 02 08 03 03
    80H: 0a 01 5a 06 00 03 22 00 00 12 1d 64 00 00 0a 04
    90H: 10 80 80 00 4c 1a 60 50 00 00 00 0a 05 05 03 bc
    A0H: bc 00 0d 02 90 01 78 00 00 08 03 d8 05 00 01 00
    B0H: 00 ff ff e4 e4 00 71 12 40 00 00 01 d7 0f 00 00
    C0H: 00 88 88 c9 01 00 00 00 00 a5 ff 7e 01 00 00 00
    D0H: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    E0H: 00 00 00 00 25 25 25 25 54 00 00 00 00 00 00 25
    F0H: 08 00 00 00 00 00 00 00 00 25 25 25 25 25 2f 01

    3. 在VIN_1口输入CVBS(PAL 彩条)

    寄存器与上相同,只是A9:变为:40。