This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c5515EMIF外扩存储时,FLASH和SDRAM地址线接线方式为什么不一样?



各位,看了EVMC5515的原理图,外扩FLASH时地址线往后错一位比如A0接A1,而扩SDRAM时,却并没有错开,A0接A0,这是为什么呢?求教。

  • 这是EMIF口接异步memory的要求。

    Of special note is the connection between the EMIF and the external device's address bus. The EMIF
    address pins EM_A[20:0] always provide the least significant bits of a double-word (32-bit) address. The
    EM_BA[1:0] pins provide word (16-bit) and byte selection functionality according to the data bus width
    configured in the Asynchronous CSn Configuration Register 1 (ACSnCR1).


    http://www.ti.com/lit/ug/sprugu6b/sprugu6b.pdf