This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6412 flash 烧写文件格式



我用的 ROM BOOT 模式,外挂8bit FLASH,  生成的hex文件部分内容如下所示:

5A A3 80 00 00 80 00 00 00 00 00 00 29 00 00 02 2A 50 10 02 69 C0 00 02 

对写入flash 的数据内容有点疑问,请各位帮忙释疑:

比如第一个数据“5A”,  从文件读出来是两个字节:一个是“5”,十六进制表示为0x35,;一个是"A",用十六进制表示为0x41

1)我是把0x35和0x41写入flash吗,还是把0x5A写入flash?

2)此外,“5A”和"A3"之间还有一个空格,从文件读出来的数据是0x20,这个需要写入flash吗?