This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用的是ti的评估版evm6670,报错信息如下:
IcePick_D: Error connecting to the target:
(Error -503 @ 0x0) The user selected phase-one auto-range frequency failed the scan-path test.
The utility or debugger requested the JTAG controller and cable, that generate the JTAG clock, to use a user selected feature or algorithm.
The built-in scan-path reliability test has failed.
This indicates that the JTAG controller and its cable cannot reliably communicate with the target system using that feature or algorithm.
Try using the legacy frequency or a known good specific frequency. (Emulation package 5.0.872.0)
看一下仿真器上的LED灯状态是否进入safemode。
When SAFE mode is active the LEDs D4, D5 and D6 will blink simultaneously.
http://processors.wiki.ti.com/images/d/df/Emulator_safemode.pdf
CCS v5.3不支持win10。用ccs v6, v7。
http://processors.wiki.ti.com/index.php/System_Requirements