新做的板子每个电源是独立供的,刚开始由于上电复位没有延时导致1.8V被拉到了2.7V现在解决这个问题后xds100仿真器连不上dsp,
测量各各电压正常,时钟输入幅度1.25V,现在测量PLL输出引脚没有输出,这个PLL输出是芯片只要正常工作就可以输出还是需要软件配置?
还有就是跟仿真连接还需要上下拉EMU0和EMU1与否?BOOT是否需要配置?
芯片1.8V被拉到2.7V是否会被损坏?
这是现在报的错
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.232.0)