大家好!请帮忙看看:
AM335x使用linux自带的SPI驱动,master模式,用示波器测试发现SPI1_D0数据线方向默认为输入,SPI1_D1数据线方向为输出。
想把SPI1_D0数据线方向配置成输出,SPI1_D1配置为输入,应该如何更改内核?先谢谢了!
AM335x的Table 24-4. McSPI Pin List中有写:SPIx_D0和SPIx_D1都能配置为输入或输出“(Can be configured as either input or output (MOSI or MISO)”,因为我硬件电路上已经做死了(SPI1_D0输出,SPI1_D1输入)。