大家好:
我想使用AM335x 做一个全速USB设备。看数据手册,AM335x支持全速和高速USB,但是在StartWare里面的程序都是高速的USB代码,请问,我应该怎么将USB设置成全速模式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
USB MSC (MUSB) Host mode EXT2 File System Performance
USB-MSC MUSB Host-DMA-Write Performance values Buffer Size (in Bytes) Transfer Rate (in MBytes/sec) CPU Load (in %)
102400 24.41 26.30
1048576 24.20 23.48
5242880 24.10 21.94
USB-MSC MUSB Host-DMA-Read Performance values Buffer Size (in Bytes) Transfer Rate (in MBytes/sec) CPU Load (in %)
102400 23.63 27.13
1048576 23.54 27.27
5242880 23.57 27.50
USB MSC (MUSB) Host mode VFAT File System Performance
USB-MSC MUSB Host-DMA-Write Performance values Buffer Size (in Bytes) Transfer Rate (in MBytes/sec) CPU Load (in %)
102400 22.61 36.55
262144 22.56 35.31
USB-MSC MUSB Host-DMA-Read Performance values Buffer Size (in Bytes) Transfer Rate (in MBytes/sec) CPU Load (in %)
102400 22.26 24.39
262144 22.02 26.95
你好,AM335X_StarterWare_02_00_01_01这个版本的device bulk传输怎么把高速USB改为全速呢???